STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trouble with TCP/IP on STM32F407ZET6 and LAN8742A

I've managed to get tcp/ip working just fine on the NUCLEO-429ZI board, but I'm unable to make similar code work on the 407ZET6 chip, despite using what I believe to be a nearly identical circuit with the LA8742A chip.  I suspected it had something t...

jermat by Associate
  • 2399 Views
  • 3 replies
  • 0 kudos

STM32H745 USB HOST and FreeRTOS CMSIS V1 problem

I have a project created with TouchGFX for STM32CubeIDE.All in latest versions and it works. The firmware pack has a support for the WM8994 audio chip as BSP driver. I lost like a month of my work trying to figure out why the driver fails randomly to...

HTD_0-1695139862909.png
HTD by Senior III
  • 1781 Views
  • 1 replies
  • 1 kudos

SBSFU Application upgrade fails

Hi,I'm working on STM32G0B0RE custom device. I have ported SBSFU through USB CDC. I'm able to program SBSFU and application. The application is working as expected but when I try to upgrade application it fails to rewrite the application header in th...

Tarun_0-1695134618462.png Tarun_0-1695135417335.png
Tarun by Associate III
  • 1034 Views
  • 0 replies
  • 0 kudos

NUCLO.H753ZI, cannot get USB device running

I'd like to activate the user USB on the NUCLO.H753ZI board, as a USB device for serial emulation (CDC)I use CUBE generated code (basic demo setup for this CPU), the ST-Link USB works and I can debug. I may add, that I have USB working with Cube-code...

VKoen.1 by Associate II
  • 1709 Views
  • 1 replies
  • 0 kudos

HAL_I2C_Mem_Read_DMA not working on STM32H723

Hi all,I have been trying to get I2C DMA working on an STM32H723 for a few days now. It works perfectly when using blocking mode (using HAL_I2C_Mem_Read), but when I try to use HAL_I2C_Mem_Read_DMA it returns success, but doesn't actually do the read...

Simon_0-1695019170931.png Simon_1-1695019340613.png
Simon by Associate III
  • 6091 Views
  • 7 replies
  • 2 kudos

LWIP MBEDTLS, no RTOS

I have tried to get LWIP and MBEDTLS working in RAW mode without an RTOS but have failed miserably...I think I have overlooked something - any suggestions?The failure is at -ssl_tls.c - line 2629if( ! mbedtls_pk_can_do( &ssl->session_negotiate->peer_...

PNG compression

Hi,i'm using the NUCLEO U575ZI-Q board I want to compress some data I collect from analog sensors via png encoding in order to take advantage of compression, how can I do it? Are there special libraries for that?I don't need to have the .png file but...

Rturo by Associate II
  • 4902 Views
  • 8 replies
  • 0 kudos

STM32G071CB Battery voltage monitoring issue

 HI. I would like to use the battery voltage monitoring feature.I am reading the ADC by connecting a DC source and adjusting the value from 2.6V to 3.6V. We tested 10 boards and they all had different ADC values.The biggest difference was over 100.PC...

songkw by Associate II
  • 1548 Views
  • 2 replies
  • 1 kudos

Resolved! Automatic Storing Data in external flash

I am running LED matrix display from F0 Series MCU. At present whatever I want to display on board, I am putting "Hex code of LED matrix" in the main loop code.  But Now I want to have USB stick containing Hex code of LED matrix. Basically user will ...

Nico3 by Senior
  • 1278 Views
  • 1 replies
  • 1 kudos