STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U5 SPI Slave Not Working Zephyr

Hi all,I'm struggling to get SPI working on my STM32U5G9J. I have an nordic master device outputting 6 bytes of data every 500 ms over SPI and plugged into the proper pins, double checked and confirmed on analyzer.stm32u5g9j_dk2.overlay/ { aliase...

rulmer by Associate II
  • 371 Views
  • 1 replies
  • 0 kudos

Resolved! USBX as a host in stand alone

Hey there at @Pavel A. I've implemented USBCDC as a device In stand alone mode successfully I intend on implementing CDC host stand alone that is to say without X-thread RTOS.The generated files from cube MX don't have Read_run and Write_run function...

Resolved! STM32F407 SPI1 over DMA2 Zephyr RTOS

Hi All,   I have been using SPI1 over DMA2 on Zephyr RTOS recently to read my external flash. I had done similar thing on Bare metal / FreeRTOS based program. Both of them work fine. However, there is a problem in Zephyr based implementation of its d...

Neolithic by Associate III
  • 508 Views
  • 5 replies
  • 1 kudos

STM32N6 VENC + NPU + Camera linker script

Hi all,I am currently trying to merge the STM32N6 VENC_SDCARD Project with my Codebase that is based on the STM32 Modelzoo Object Detection (https://github.com/AlexGraefe/STM32N6CameraEvaluation). However, naively copy-pasting the code does not work....

devjalx by Associate II
  • 222 Views
  • 2 replies
  • 0 kudos

USB CDC Host SetControlLineState

HiCan anyone please show me an example of a working USB CDC Host sending the SetControlLineState command? This hasn't been implemented in the STM32 HAL drivers/middleware but it should be a simple thing to add.SetControlLineState is used to signal t...