Skip to main content
Visitor II
April 2, 2025
Question

Switching Between USB Host and Device Modes on STM32F769I-DISCO using a button

  • April 2, 2025
  • 3 replies
  • 740 views

Hello,

I am working with an STM32F769I-DISCO board and trying to implement functionality that allows switching between USB Host and Device modes via a button press. I have configured the board for OTG/Dual Role in STM32CubeMX, but I did not enable the Middleware for USB Host or USB Device, so I need to manage the switching at the register level and using HAL APIs.

I would appreciate any advice or code examples for properly managing this switch:

  1. Initialization: How should I correctly initialize the USB peripheral to support both modes (Host and Device)?

  2. Mode Switching: What are the recommended steps to deactivate one mode and activate the other without causing conflicts or stability issues?

  3. Specific APIs and Registers: Are there specific HAL APIs to use, or do I need to manipulate the registers directly? If so, which are most relevant for this purpose?

I've attempted to implement a basic switch using HAL_PCD_Stop() and HAL_HCD_Start(), but I'm not sure if this is the best approach. Also, I am open to suggestions to ensure a smooth and stable transition between modes.

Any help or direction would be greatly appreciated!

Thank you in advance,

This topic has been closed for replies.

3 replies

KORKAD
ST Technical Moderator
May 20, 2025

Hello @bogdanys 

You can start with the USB Host or Device applications available within the STM32CubeF7 V1.17.0 firmware package. This package is available for download from the ST website and GitHub.

STM32CubeF7 - STM32Cube MCU Package for STM32F7 series (HAL, Low-Layer APIs and CMSIS, USB, TCP/IP, File system, RTOS, Graphic - and examples running on ST boards) - STMicroelectronics

Regards,

ABOUA
ST Employee
May 20, 2025

Hello,

USB dual role on STMF7 can be enabled, you should ensure to DeInit the USB resources either for HAL and MW before switching the role

Regards 

ST Technical Moderator
May 23, 2025

Hello @bogdanys 

I have attached a project that supports dual role data on an H723ZG Nucleo board. This project switches modes with  user button . It may help you configure mode switching on your board.

To initialize  modes correctly, you need to add device and host-related files to your project and use the middleware initialization function of the desired mode.

To execute mode switching, you can use specific functions available in the middleware files, such as USBD_Init, USBD_DeInit, USBH_Init, and USBH_DeInit along  drive vbus functions.

 

Gyessine

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.