STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 V2Link

Hello, I have been trying to program a custom board.  I am using the stm32f042k6t7 chip and I have been working on this for a few weeks now.  I've got my board double checked and even ordered another V2Link thinking it might be that connector.  I hav...

schleise by Associate
  • 1335 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F401 SPI CLK not working

Hi guys,I'm currently working on a project where I need to use the SPI protocol. After setting everything up in the .ioc file and generating the code. I wanted to check if the clock signal was properly working. So i hooked up my ossciloscop to the cl...

djerikos by Associate II
  • 6354 Views
  • 5 replies
  • 5 kudos

Resolved! Stop mode in STM32G0

Dear All,I'm using stm32G0 MCU for battery operated application and I2C,  UART and RTC and GPIO are using I want know What should be peripheral state before going to STOP mode mean "should be deinit before going to stop mode or leave it as it is and ...

vchau.2 by Associate III
  • 3207 Views
  • 3 replies
  • 4 kudos

DCMI Crop feature

Hi all, I recently started learning about st-controllers and I am stuck in this, any help would be greatly appreciated.I am working with stmf746, I wanted to crop the captured image with DCMI crop feature, I am configuring crop window size and offset...

lglad by Associate
  • 2707 Views
  • 3 replies
  • 1 kudos

PWM phase shift for dual active bridge

I have a dual active bridge and I am supposed to do leading and lagging phase shift to achieve that. This needs to be a precise shift to the lowest degree of 1. I am using an STM32F429. This is the logic I am using:HAL_TIM_PWM_Start(&htim3, TIM_CHANN...

Gaia by Associate
  • 946 Views
  • 0 replies
  • 0 kudos

USB CDC works on STM32G431 but not STM32L151

Hi, I am trying to setup USB CDC as virtual COM port on STM32L151. I just enabled it through cubeMX and connected the wires. Windows keep saying device not recognized.I just did the exact same thing with STM32G431. An empty project with just USB CDC ...

HKaze.2 by Associate
  • 1655 Views
  • 2 replies
  • 0 kudos

Resolved! Upgrade from STM32L432KB to STM32L432KC

Hi Everyone,I'm upgrading our firmware from STM32L432kb with 128k flash memory to STM32L432KC with 256k flash memory. both micro controllers are  exactly the same except for the flash memory size difference. To accommodate this change I changed my co...

RTOS Task management "architecture"

Hello everyone.This is more of a general RTOS question regarding the approach of task management. I've got everything pretty much working but im certain there is a better solution than mine. I'm using FreeRTOS with the CMSIS v2 wrapper.Background:The...

XD by Associate III
  • 1931 Views
  • 0 replies
  • 0 kudos