STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB-Host with STM32U5 and ThreadX

Hi, I try to get the USB-Host running with USBX. Hardware is a custom board with TCPP02 and STM32U575. Init process is running, but I never get an interrupt (ux_host_event_callback) when plugging in a USB stick. Any idea? ioc file and schematic are a...

AWack by Senior
  • 237 Views
  • 5 replies
  • 0 kudos

EPR request in STM32G071

HelloI have my own board with STM32G071KBT6 microcontroller. I successfully comunicate with charger by PD protocol and I receive up to 21 V (PPS). But I need above 21V. I have power bank with AVS up to 28V and USB cable with e-marker (up to 240W). Ho...

NUCLEO-H7S3L8 debug problems

Hello, Started to dwell info embedded development and got my hands on a NUCLEO-H7S3L8 development board. Firstly wanted to analyze the example code that comes with the development board and modify it a bit. But when started to debug, it seems to stop...

Domi by Associate
  • 130 Views
  • 2 replies
  • 0 kudos