STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Questions about PDM MEMS microphones.

I am using STM32F407 Discovery Board for my audio project. There is a PDM mems microphone on this board. I want to get sound signal over I2S with DMA. For that ı am using SWV graph in İDE. I tried all ı found on the internet. ı have a few questions t...

Trampler_0-1707135217960.png 1707133719056.jpg Trampler_1-1707135391085.png Trampler_2-1707135399453.png
Trampler by Associate III
  • 2428 Views
  • 1 replies
  • 0 kudos

Resolved! xQueueSemaphoreTake() hangs for ever

Hi all,I have a problem on my current design. My setup... .I have a mqtt client connected to a broker. I use the lwip library together with freertos STMCube provides. So it's mainly default. I have one task for sending and receiving. Now all works fo...

MOtto.1 by Associate II
  • 2185 Views
  • 1 replies
  • 0 kudos

Resolved! exFAT support for FileX on STM32U5

I'm testing out using an SD card on the STM32U575I-EV. The example project I'm using is from the STM32CubeU5 MCU package (Projects\STM32U575I-EV\Applications\FileX\Fx_uSD_File_Edit).I'm able to insert an SDHC (32GB; FAT32 format) card, see the green ...

Resolved! G071 TIM2 CH3 PWM output not starting

I'm sure I'm missing something here but for the life of me I can't see it.TIM2 CH1+CH2 are in use as encoder inputs but I believe I should still be able to generate a basic PWM output on CH3 at the same time?Code is all generated by Cube IDE and it r...

JU by Senior
  • 3753 Views
  • 3 replies
  • 2 kudos

EMMC and power consumption

HiI have a custom board with an EMMC connected STM32F446.My write access to EMMC for 16 kbytes is quite fast (2-3 ms). EMMC during the write operation consumes some 50 milli ampere more than during the its idle state. This would be fine, but as far a...

MK..1 by Senior
  • 4050 Views
  • 4 replies
  • 0 kudos