STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! G071 TIM2 CH3 PWM output not starting

I'm sure I'm missing something here but for the life of me I can't see it.TIM2 CH1+CH2 are in use as encoder inputs but I believe I should still be able to generate a basic PWM output on CH3 at the same time?Code is all generated by Cube IDE and it r...

JU by Senior
  • 3760 Views
  • 3 replies
  • 2 kudos

EMMC and power consumption

HiI have a custom board with an EMMC connected STM32F446.My write access to EMMC for 16 kbytes is quite fast (2-3 ms). EMMC during the write operation consumes some 50 milli ampere more than during the its idle state. This would be fine, but as far a...

MK..1 by Senior
  • 4058 Views
  • 4 replies
  • 0 kudos

STM32F4 USART Bootloader

We have been building boards for years using the STM32F407ZET6. Our system uses a USART bootloader from a host processor running Android that uses stm32ld to do the bootloading. It has worked pretty much flawlessly for years. Recently we started rece...

I2C Slave NUCLEO-F411RE

Hello,  I am currently working on a project where I need to configure a NUCLEO F411RE Board as an I2C slave. It will be connected to a Raspberry Pi Master. I am able to detect the NUCLEO on the raspberry Pi, however I am unsure how to get the read by...

dae by Associate II
  • 4669 Views
  • 8 replies
  • 2 kudos

Problem Restarting full duplex SPI DMA on STM32G474

Good morning everyone,I have an application where a STM32G474 as SPI master interacts with another ST controller as SPI slave. These are full-duplex DMA transfers of about 500 bytes at 10MBit transfer rate. The slave signals that it is alive via a di...

SRond by Associate III
  • 5527 Views
  • 8 replies
  • 4 kudos

Resolved! STM32F4 Serial Port Forwarding Architecture

 The system consists of three modules: a 4G module, a GNSS module, and an STM32 processor, with the modules connected to the STM32 via UART. In terms of program functionality, the STM32 needs to implement data forwarding and saving. It receives data ...

WinstonTom_4-1707224984402.png WinstonTom_5-1707224990433.png

How to flash STM32H725 using FDCAN Bootloader?

I went through the following documentation available from STM on FDCAN bootloader:AN5405 - FDCAN protocol used in the STM32 bootloaderAN2606 - STM32 microcontroller system memory boot moderm0468 - Reference manualJump to bootloader code used: (Refere...

_legacyfs_online_stmicro_images_0693W00000bl8iSQAQ.png _legacyfs_online_stmicro_images_0693W00000bl8iwQAA.png
1080P by Associate
  • 3135 Views
  • 2 replies
  • 2 kudos