STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Missing out byte while receiving data on UART

Hi Community,I am working in a freeRTOS environment where one of the threads parses the serial data from the UART. A protocol is defined to decode the hex stream received from another device. HAL_UART_RxCpltCallback is configured to receive one byte ...

Resolved! HAL_TIMEOUT error from HAL_RCC_OscConfig()

Hi,my app works fine when I use the internal clock but if I switch to external clock I obtain HAL_TIMEOUT from function HAL_RCC_OscConfig().The external clock board schematic is:Clock configuration is:The main.c is:   /* USER CODE BEGIN Header */ /**...

screen_3.jpg screen_1.jpg screen_2.jpg
Beppe101 by Associate III
  • 3073 Views
  • 4 replies
  • 2 kudos

Resolved! Code Isolation on STM32G484VET for safety-critical (non-upgradable area) and non-safety-critical (Upgradable area)

Hello Support Team.Good Day.We have chosen the STM32G484VET controller for our product.According to the firmware architecture, we intend to create two separate partitions, one for safety-critical (non-upgradable area) and the other for non-safety-cri...

Resolved! There is a problem that USBPD_CAD_Task stops

 Hello,I am developing a USB Type C chargerThe development environment is as follows HardwareNUCLEO-G071RB (tested on rev C)X-NUCLEO-DRP1M1 shield Softwarex-cube-tcppDRP1M1_DRP When this board is connected to a Windows tablet, the CAD task(USBPD_CAD_...

forst by Associate III
  • 4936 Views
  • 4 replies
  • 1 kudos

DP83822 instead of DP83848

Has anyone written a driver for the DP83822 PHY ?I have tried to use the DP83848 driver. I am able to pass the DP83848_Init(&DP83848); in the ethernetif.c but then when it comes to check the list status, then I get a link down status. The LEDs on my ...

Resolved! Free RTOS queue mechanism does not work as expected.

Hi,I have created two tasks. Task A and Task B. Task A has higher priority. Task receives data through UART and enques this data into queue. Then, Task A is blocked for 1 second. Task B comes into picture and dequeues the data from queue. I send 8 by...

demir_0-1710088589010.png demir_1-1710088719866.png demir_0-1710089346378.png
demir by Senior II
  • 1836 Views
  • 1 replies
  • 1 kudos

Transmitting and receiving custom serial bitstream

Hi Community, 1) I have to demodulated a continuous bitstream of 201bit (1ms per bit) sent by a host to my stm32F401RE. Which peripheral would you suggest to use?2) If I have to transmitt and receive custom serial data  in half duplex with clock in T...

FAJOL.1 by Associate III
  • 2390 Views
  • 4 replies
  • 0 kudos

Using LwIP's sockets with CubeMX ?

I would like to use plain sockets in my non OS STM32 application.  LwIP provides plain sockets.  I have used them in ESP32 applications where they work well.LwIP sockets are not an option in CubeMX as far as I can tell.   One can manually enable sock...

Someguy by Associate III
  • 2635 Views
  • 2 replies
  • 2 kudos