STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32U073 LPUART not waking from STOP2

Hello,I'm working on a low power project using STM32U073 with FreeRTOS, LPUART2 and LPTIM1.To achieve the lowest system power possible I am trying to use STOP2 for when the system is idle.Currently I have LPTIM1 releasing a semaphore every 1 second w...

Getting HAL_Delay() working in external loader

Hello, i created a custom external loader for a STM32F429 board.The problem is now, my code needs HAL_Delay() for generating short delays between flash device accesses. And the code freezes when executing HAL_Delay(). So i have read that interrupts a...

sk-st by Associate III
  • 296 Views
  • 3 replies
  • 0 kudos

Resolved! LwIP STM32h723zg

Hello.I've tried to implement the TCP client using freeRTOS, socekt API and LwIP middleware on STM32H723ZG.However, I cannot figure out why the connect() function in socket api doesn't work and stuck.Is there a example for nucleo-H723ZG with LwIP and...

USBX Host MSC Standalone functions missing

I am on an H562 and trying to rd/wr a file on a USB memory stick using the mass storage controller. I am trying to understand what to do about this block when I am running in standalone mode. I started from an example code which is in RTOS mode but I...

Capocc_1-1763462236696.png Capocc_2-1763462321952.png Capocc_3-1763462637638.png
Capocc by Associate II
  • 519 Views
  • 6 replies
  • 1 kudos