cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6 timer One Pulse Mode with external trigger

PeterPan
Associate II

Hello

I have custom board with STM32N657. I have set timer 2 to output PWM pulse on channel3 and output compare pulse on channel 1 as trigger to another timer. The timer starts when external trigger - TIMER4_ETR (mapped to timer 2) detects rising edge. All works good, there are continuous pulses as expected.

I want timer2 to run once per trigger so enabling One Pulse Mode. 

static void MX_TIM2_Init(void)
{

  /* USER CODE BEGIN TIM2_Init 0 */

  /* USER CODE END TIM2_Init 0 */

  TIM_ClockConfigTypeDef sClockSourceConfig = {0};
  TIM_SlaveConfigTypeDef sSlaveConfig = {0};
  TIM_MasterConfigTypeDef sMasterConfig = {0};
  TIM_OC_InitTypeDef sConfigOC = {0};

  /* USER CODE BEGIN TIM2_Init 1 */

  /* USER CODE END TIM2_Init 1 */
  htim2.Instance = TIM2;
  htim2.Init.Prescaler = TIM2_PRESCALER;
  htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
  htim2.Init.Period = TIM2_PERIOD;
  htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
  htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
  if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
  {
    Error_Handler();
  }
  sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
  if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
  {
    Error_Handler();
  }
//  if (HAL_TIM_OC_Init(&htim2) != HAL_OK)
//  {
//    Error_Handler();
//  }
//  if (HAL_TIM_PWM_Init(&htim2) != HAL_OK)
//  {
//    Error_Handler();
//  }
  if (HAL_TIM_OnePulse_Init(&htim2, TIM_OPMODE_SINGLE) != HAL_OK)
   {
     Error_Handler();
   }
  sSlaveConfig.SlaveMode = TIM_SLAVEMODE_TRIGGER;
  sSlaveConfig.InputTrigger = TIM_TS_ETRF;
  sSlaveConfig.TriggerPolarity = TIM_TRIGGERPOLARITY_NONINVERTED;
  sSlaveConfig.TriggerPrescaler = TIM_TRIGGERPRESCALER_DIV1;
  sSlaveConfig.TriggerFilter = 0;
  if (HAL_TIM_SlaveConfigSynchro(&htim2, &sSlaveConfig) != HAL_OK)
  {
    Error_Handler();
  }
  HAL_TIMEx_RemapConfig(&htim2, TIM_TIM2_ETR_TIM4_ETR);
  sMasterConfig.MasterOutputTrigger = TIM_TRGO_OC1;
  sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_ENABLE;
  if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
  {
    Error_Handler();
  }

  sConfigOC.OCMode = TIM_OCMODE_TOGGLE;
  sConfigOC.Pulse = TIM2_PULSE_CH1;
  sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;
  sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;
  if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_1) != HAL_OK)
  {
    Error_Handler();
  }
  __HAL_TIM_ENABLE_OCxPRELOAD(&htim2, TIM_CHANNEL_1);
  sConfigOC.OCMode = TIM_OCMODE_PWM1;
  sConfigOC.Pulse = TIM2_PULSE_CH3;
  sConfigOC.OCPolarity = TIM_OCPOLARITY_LOW;
  if (HAL_TIM_PWM_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_3) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN TIM2_Init 2 */

  TIM_CCxChannelCmd(htim2.Instance, TIM_CHANNEL_1, TIM_CCx_ENABLE);
  TIM_CCxChannelCmd(htim2.Instance, TIM_CHANNEL_3, TIM_CCx_ENABLE);

  /* USER CODE END TIM2_Init 2 */
  HAL_TIM_MspPostInit(&htim2);

}

//Then in main
HAL_TIM_Base_Start_IT(&htim2);

The above code configures timer2 to OPM mode but no output pules are generated when triggered.
When clearing OPM bit, TIM2->CR1 &= ~TIM_CR1_OPM, and starting timer with external trigger then output channels generate pulses again so configuration seems to be correct in non-OPM mode.

Any suggestion where might be a problem?

Examples show how to configure OPM with TIxFPx trigger but non with external trigger.

1 REPLY 1
Francois VILMAIN
ST Employee

Hello,

did you check that he following condition is met (refer to RN0486, section:50.3.22)

FrancoisVILMAIN_0-1763564722031.png