STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Type-C IC suggestion

Hi,I'm looking for some suggestions for the implementation of a self-powered and DRD (Dual Role Data) system provided with USB Type-C connector, but without PD support.I found two different solutions:1) Using a configuration channels protection IC (T...

__NVIC_EnableIRQ Can not enable TIM2

I'm learning to port FreeRTOS to my STM32F407, but I'm running into problems with HAL initializing TIM2.After HAL_OK the program is supposed to enable TIM2IRQ via NVIC_EnableIRQ(), but the operation of writing to NVIC->ISER doesn't seem to work.NVIC-...

Jemegen by Associate III
  • 2484 Views
  • 4 replies
  • 0 kudos

STM32 CDC Host with Custom baud rate

I've created a project with STM32F407xxx, and using as USBH_CDC with this MCU. STM is working fine but the problem is, the baud rate can not be edited. It is auto by default. How can I keep it fixed at a certain baud rate such as 9600 or 115200? I tr...

MKDas by Associate II
  • 5487 Views
  • 8 replies
  • 0 kudos

Resolved! How to enable DMA mode to transfer data using SDIO

Posted on May 26, 2017 at 06:18 Hello, I am using STM32F411RET6 chip to access uSD card with SDIO 4bit. By default it uses polling mode to read/write data with SDIO, such asBSP_SD_ReadBlocks(). The problem is that I want to continuously wri...

rwmao by Senior
  • 3202 Views
  • 4 replies
  • 0 kudos

Connecting STM32F7 DISCO to WiFi Using ESP8266

Hello everyone,I'm currently facing an issue with migrating an ESP8266 project from EWARM IDE to CUBE IDE for use with the STM32F769I-DISCO board for WiFi connection.When attempting to open the project from the example selector in CUBE MX, I received...

NB1 by Associate II
  • 2019 Views
  • 3 replies
  • 5 kudos

ETH and LwIP memories configurations

Hi there!I already configured LwIP package and make it work on a NUCLEO-H755ZIQ following @Adam BERLINGER gude in the Knowledge base section.Even if the communication is working, some configurations are to me totally cryptic...In particular, I would ...

iTTy_0-1712837348043.png iTTy_1-1712837663959.png
iTTy by Senior
  • 1561 Views
  • 1 replies
  • 2 kudos

i2s driver audio chip

Hello, I am a student. I want to use I2S through STM32L051K8U6N to complete the acquisition of the MP34DT04 sensor, but I have not found any information about libPDMFilter_CM4F_Keil.lib, keil library and IAR library similar to this. If it is convenie...

Daqiang by Associate II
  • 1196 Views
  • 0 replies
  • 0 kudos