STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SDMMC + FATFS on STM32H753Zx

Hi,   i go to start SDMMC1 in STM32H753z, is any sample code? can please provide.   in SDMMC i need to use FATFS APIs or SDMMC APIs ? i am confusing please help me.   when i debug the below code i am can n't access it stop at f_mount() starting only....

Naresh_ by Associate III
  • 4567 Views
  • 6 replies
  • 0 kudos

STM32 LPUART INTERRUPT IS NOT WORKING

Hi,I am developing on stm32l011 board and I am facing issue about UART interrupt. static uint8_t rxBuffer[32] = { 0 }; void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart) { /* Check if it is start command. */ if(NULL != strstr((char*) rxBuffer,...

processing audio in real time

In the next code I sample audio from the mic, play it to the headphones, then i process the data to get Mel-Spectrogram feature and then I feed the Mel feature into an AI model to recognize speech.when I enable the functions that calc the mel and the...

audi by Associate II
  • 2445 Views
  • 4 replies
  • 1 kudos

Resolved! STM32H723 software framework

I want to develop an inverter with STM32H723, but I have not used ST's MCU for power supply before, so I would like to ask if there are suitable examples for reference, or what suggestions are there in the software framework. Thank you!

buxiang by Associate
  • 1410 Views
  • 1 replies
  • 0 kudos

STM32U585OIY6QTR ADC

The ADC seem to work when i run this code.Internal ADC like vref vbat and internal temperature seem to be working and I testes it with cold spay and checked the internal temperature.the ADC input pins seem to be stuck ate a level and not change or gi...

Certified RTOS for STM32

Hi,I have general question. What certified RTOS do you recommend for using in medical device running on STM32F/G/H that will be certified in accordance with IEC 62304 Class C?Best regards,KK

kk2 by Associate III
  • 2070 Views
  • 4 replies
  • 3 kudos