STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32G4xx HAL Driver V1.2.5 Issue with DMAMUX

Hello ST,I would like to report a bug in the <stm32g4xx_hal_dma.c> file (V1.2.5). In the function DMA_CalcDMAMUXChannelBaseAndMask(DMA_HandleTypeDef *hdma), there's an error in calculating hdma->DMAmuxChannelStatusMask. For DMA2 channels, the channel...

Penguins by Associate
  • 508 Views
  • 4 replies
  • 0 kudos

Resolved! USBX Audio Class frame done callback not called

Please refer to this thread that, for some reason, @FBL accepted as an answer (it is not) https://community.st.com/t5/stm32-mcus-embedded-software/usbx-audio-class-frame-done-callback-not-called/td-p/855262I'm seeing that when I try to start an audio...

nico23 by Senior III
  • 303 Views
  • 3 replies
  • 0 kudos

Resolved! Best way to configure ADC reading for speed

Hello, I am trying to configure my STM32H723ZG to be able to read the value of a few current sensors. My main concern at the moment is the speed at which I need to read these. I'm hoping to be reading upwards of rate of 20kHz. My questions are about ...

evanpol by Associate III
  • 853 Views
  • 7 replies
  • 2 kudos

Resolved! Refined Ticket for ST Community

Hi ST Team,I am currently using STM32H563ZIT6 and STM32H755ZIT6 in my project. We are now preparing to move from prototype to mass production, with an estimated requirement of ~10,000,000 units per year.As we transition into production, I am facing s...

Get back in IAP from APP

Hello,Im beginner,STM32H753 on the EVAL BOARD,Objective:At startup, the IAP is ignored with a condition on the jumpToIAPFlag flag that checks whether the reset is related to POWER ON or NRST (hardware button), which would therefore be a normal startu...

HugoSTM32 by Associate III
  • 834 Views
  • 12 replies
  • 6 kudos