2025-06-19 10:30 AM
Hello ST,
I would like to report a bug in the <stm32g4xx_hal_dma.c> file (V1.2.5). In the function DMA_CalcDMAMUXChannelBaseAndMask(DMA_HandleTypeDef *hdma), there's an error in calculating hdma->DMAmuxChannelStatusMask. For DMA2 channels, the channel_number should be adjusted by adding 8, 6, or 7 according to the MCU category. Otherwise, it will NOT be able to correctly determine and clear the synchronization overrun interrupt of the corresponding channel.
To give you a better understanding of the issue, I've included some relevant code snippets with comments at Line 32 below:
/**
* @brief Updates the DMA handle with the DMAMUX channel and status mask depending on stream number
* @PAram hdma pointer to a DMA_HandleTypeDef structure that contains
* the configuration information for the specified DMA Stream.
* @retval None
*/
static void DMA_CalcDMAMUXChannelBaseAndMask(DMA_HandleTypeDef *hdma)
{
uint32_t dmamux_base_addr;
uint32_t channel_number;
DMAMUX_Channel_TypeDef *DMAMUX1_ChannelBase;
/* check if instance is not outside the DMA channel range */
if ((uint32_t)hdma->Instance < (uint32_t)DMA2_Channel1)
{
/* DMA1 */
DMAMUX1_ChannelBase = DMAMUX1_Channel0;
}
else
{
/* DMA2 */
#if defined (STM32G471xx) || defined (STM32G473xx) || defined (STM32G474xx) || defined (STM32G414xx) || defined (STM32G483xx) || defined (STM32G484xx) || defined (STM32G491xx) || defined (STM32G4A1xx) || defined (STM32G411xC)
DMAMUX1_ChannelBase = DMAMUX1_Channel8;
#elif defined (STM32G411xB) || defined (STM32G431xx) || defined (STM32G441xx) || defined (STM32GBK1CB)
DMAMUX1_ChannelBase = DMAMUX1_Channel6;
#else
DMAMUX1_ChannelBase = DMAMUX1_Channel7;
#endif /* STM32G4x1xx) */
}
dmamux_base_addr = (uint32_t)DMAMUX1_ChannelBase;
channel_number = (((uint32_t)hdma->Instance & 0xFFU) - 8U) / 20U;
/** Code should be added here to distinguish DMA2 channels from DMA1 ones. **/
hdma->DMAmuxChannel = (DMAMUX_Channel_TypeDef *)(uint32_t)(dmamux_base_addr + ((hdma->ChannelIndex >> 2U) * ((uint32_t)DMAMUX1_Channel1 - (uint32_t)DMAMUX1_Channel0)));
hdma->DMAmuxChannelStatus = DMAMUX1_ChannelStatus;
hdma->DMAmuxChannelStatusMask = 1UL << (channel_number & 0x1FU);
}Best regards,
Penguins
Solved! Go to Solution.
2025-06-20 3:40 AM
Hello @Penguins
Thank you for bringing this to our attention
I reported this internally
Internal ticket number: 212655 (This is an internal tracking number and is not accessible or usable by customers).
2025-06-20 3:40 AM
Hello @Penguins
Thank you for bringing this to our attention
I reported this internally
Internal ticket number: 212655 (This is an internal tracking number and is not accessible or usable by customers).
2025-11-22 12:03 AM
I noticed that this issue has not been fixed yet.
2025-11-24 12:23 AM
Hello @Penguins
The fix is scheduled to be released on GitHub soon.
2025-11-28 5:49 AM
Hello @Penguins
The fix has been released and now available on Github on the link below: