STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST UCPD Problem with capabiltity mismatch

Hello, Im trying to get a USB PD 3.0 connection betwe en an ST X-Nucleo-DRP1M1() and an power bank or wall adapter.If i ask for the source to give its capabilties, and set up an 5, 9,12, 15 or 20V Vbus voltage the nucleo says it has an capability mis...

NKramer_0-1725623496843.png
NKramer by Associate II
  • 2856 Views
  • 4 replies
  • 1 kudos

filex and directory/files

Hallo, this is my code. I create a directory, and then a file in this directory. If, in another point of the code, I check if the file is present or not, I can read/write it correctly and so on. Instead, if I stop the execution of the program, when I...

IVent.1 by Senior
  • 3482 Views
  • 6 replies
  • 0 kudos