STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Send Ping from stm32767zi

I'm utilizing two nucleo f767zi boards with the goal to get them to ping eachother using Ethernet with lwip and no RTOS. Both their Ethernet cables are connected to a switch which is also connected to my PC. With cubeide I've successfully pinged the ...

Enable ARP Offload on STM32H745

Hi,I try to enable the hardware ARP Offload in a STM32H745. The problem is, that it doesn't take the given IP adresse in die MACARPAR register regardless what the sequence of code is. I tryed it before and after enabling the ARPEN bit and before and ...

Jiahong_0-1723684351339.png
Jiahong by Associate II
  • 2287 Views
  • 3 replies
  • 0 kudos

NetXDuo issues after power loss

Hello,I have encountered a peculiar problem and I am running out of ideas on what to do next.I'm working on a project with an stm32H563 mcu and lan8742 phy, using threadX and netXduo.When the code is first downloaded it runs fine, but after a power c...

olaan by Associate II
  • 12617 Views
  • 14 replies
  • 4 kudos

STM32 HAL Macro functions

Hi everyone,I’ve noticed that STM32 drivers make extensive use of macros, and I’m curious about the reasoning behind this. Is the primary motivation is to increase performance / improve maintainability / are there other factors involved?

sarun by Associate III
  • 12573 Views
  • 23 replies
  • 10 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.