STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeMX FreeRTOS and __weak

Posted on September 13, 2017 at 14:49When enabling the FreeRTOS idle hook STM32CubeMX generates a function with the following prototype in the freertos.c file:__weak void vApplicationIdleHook( void )However __weak isn't defined in any one of the inc...

USB PTP API documentation

Hello,I'm trying to do a proof of concept using the STM32429I-EVAL1, which basically sends a PTP command to a camera. All the USB host library documentation only covers MTP, but there is nothing about PTP. I understand that this board offers out of t...

PWM shutdown using internal comparator

 Hi im using stm32g474vet6 mcu , in that im using internal comparator for PWM SHUTDOWN for protection purpose.im using comp4. comp4 input pin is directly shorted to ADC pin and reference voltage is giving using DAC.in the below attached image yellow ...

How to enable I2C - STM32F411

how to activate I2CGood morningI'm trying to make a project that requires the I2C1 bus workif I load the compiled project on arduinofrom debug the application crashes because it can't read the EEPROM on RTCI've read various documents but I can't unde...

ezioall by Associate II
  • 4744 Views
  • 5 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.