STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Help building from STM32CubeF3

Hello there! I'm trying to build a blinky program using make I'm using HAL, and the CMSIS V2 FreeRTOS ports/sources from https://github.com/STMicroelectronics/STM32CubeF3/tree/master My program compiles, but it doesn't blink, and I have no idea of ho...

laplaga by Associate II
  • 2919 Views
  • 5 replies
  • 0 kudos

Resolved! Does STM32 provide any generic VID and PID?

Hello,We are currently developing a device based on STM32L0 MCU. We would like to implement a USB device functionality in it. The problem we have is that we don't know what USB VID and PID to set for it, since we don't want to buy our own, since this...

SD Card remove and reinsert

fresult1 = f_mount(&myFATAFS, SDPath, 1) while(FR_OK != fresult1){If I remove and reinsert the SD card the f_mount return FR_DISK_ERR instead FR_OK.If I restart the project all is OK.I have the SD_CARD present pin, what can i do when the card is disc...

IlConte by Associate III
  • 3423 Views
  • 3 replies
  • 0 kudos

Ethernet DMA RBU & TBU Error bit on STM32H5

Hey there!I've been playing around with the Ethernet HAL driver on the NUCLEO-H563ZI and I was able to make it work. I'm currently using the latest STM32CubeH5 package release. Here's the issue: whenever I receive an ethernet packet, the interrupt at...

nunokisi by Associate II
  • 3078 Views
  • 2 replies
  • 0 kudos

Resolved! stm32 timer stops after integer overflow.

Hello, i have a stm32wb15cci'm trying to make a hold button, that toggles a led on/off when pressed for 2 seconds. my HCLK1 is running at 4Mhz and my prescaler is at 3999, meaning it should count up every 1ms. I'm using TIM1 which is a 16bit timer, s...

cosmtrox by Associate
  • 1540 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.