Skip to main content
Associate
November 4, 2024
Question

Help building from STM32CubeF3

  • November 4, 2024
  • 5 replies
  • 1473 views

Hello there! I'm trying to build a blinky program using make

I'm using HAL, and the CMSIS V2 FreeRTOS ports/sources from https://github.com/STMicroelectronics/STM32CubeF3/tree/master

My program compiles, but it doesn't blink, and I have no idea of how to debug it.

I'm using GCC as my compiler, this is an example of the settings I configured.

 

arm-none-eabi-gcc -c -mcpu=cortex-m4 -mthumb -mfpu=fpv4-sp-d16 -mfloat-abi=hard -DUSE_HAL_DRIVER -DSTM32F303xE -IrobotConfig/inc -I/opt/STM32CubeF3/Drivers/STM32F3xx_HAL_Driver/Inc -I/opt/STM32CubeF3/Drivers/STM32F3xx_HAL_Driver/Inc/Legacy -I/opt/STM32CubeF3/Drivers/CMSIS/Device/ST/STM32F3xx/Include -I/opt/STM32CubeF3/Drivers/CMSIS/Include -Iapp/inc -I/opt/STM32CubeF3/Middlewares/Third_Party/FreeRTOS/Source/include -I/opt/STM32CubeF3/Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS_V2 -I/opt/STM32CubeF3/Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -Og -Wall -fdata-sections -ffunction-sections -g -gdwarf-2 -MMD -MP -MF"build/stm32f3xx_ll_adc.d" -Wa,-a,-ad,-alms=build/stm32f3xx_ll_adc.lst /opt/STM32CubeF3/Drivers/STM32F3xx_HAL_Driver/Src/stm32f3xx_ll_adc.c -o build/stm32f3xx_ll_adc.o

 

This is my FreeRtosConfig, I got it from the examples, and added  the static allocation.

 

/*
 * FreeRTOS Kernel V10.0.1
 * Copyright (C) 2017 Amazon.com, Inc. or its affiliates. All Rights Reserved.
 *
 * Permission is hereby granted, free of charge, to any person obtaining a copy of
 * this software and associated documentation files (the "Software"), to deal in
 * the Software without restriction, including without limitation the rights to
 * use, copy, modify, merge, publish, distribute, sublicense, and/or sell copies of
 * the Software, and to permit persons to whom the Software is furnished to do so,
 * subject to the following conditions:
 *
 * The above copyright notice and this permission notice shall be included in all
 * copies or substantial portions of the Software.
 *
 * THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR
 * IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS
 * FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR
 * COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER
 * IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN
 * CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE.
 *
 * http://www.FreeRTOS.org
 * http://aws.amazon.com/freertos
 *
 * 1 tab == 4 spaces!
 */
#ifndef FREERTOS_CONFIG_H
#define FREERTOS_CONFIG_H

/*-----------------------------------------------------------
 * Application specific definitions.
 *
 * These definitions should be adjusted for your particular hardware and
 * application requirements.
 *
 * THESE PARAMETERS ARE DESCRIBED WITHIN THE 'CONFIGURATION' SECTION OF THE
 * FreeRTOS API DOCUMENTATION AVAILABLE ON THE FreeRTOS.org WEB SITE.
 *
 * See http://www.freertos.org/a00110.html.
 *----------------------------------------------------------*/

/* Ensure stdint is only used by the compiler, and not the assembler. */
#if defined(__ICCARM__) || defined(__CC_ARM) || defined(__GNUC__)
#include <stdint.h>
extern uint32_t SystemCoreClock;
#endif

#define configSUPPORT_STATIC_ALLOCATION 1

#define configUSE_PREEMPTION 1
#define configUSE_IDLE_HOOK 0
#define configUSE_TICK_HOOK 0
#define configCPU_CLOCK_HZ (SystemCoreClock)
#define configTICK_RATE_HZ ((TickType_t)1000)
#define configMAX_PRIORITIES (7)
#define configMINIMAL_STACK_SIZE ((uint16_t)128)
#define configTOTAL_HEAP_SIZE ((size_t)(2 * 1024))
#define configMAX_TASK_NAME_LEN (16)
#define configUSE_TRACE_FACILITY 1
#define configUSE_16_BIT_TICKS 0
#define configIDLE_SHOULD_YIELD 1
#define configUSE_MUTEXES 1
#define configQUEUE_REGISTRY_SIZE 8
#define configCHECK_FOR_STACK_OVERFLOW 0
#define configUSE_RECURSIVE_MUTEXES 1
#define configUSE_MALLOC_FAILED_HOOK 0
#define configUSE_APPLICATION_TASK_TAG 0
#define configUSE_COUNTING_SEMAPHORES 1
#define configGENERATE_RUN_TIME_STATS 0

/* Co-routine definitions. */
#define configUSE_CO_ROUTINES 0
#define configMAX_CO_ROUTINE_PRIORITIES (2)

/* Software timer definitions. */
#define configUSE_TIMERS 0
#define configTIMER_TASK_PRIORITY (2)
#define configTIMER_QUEUE_LENGTH 10
#define configTIMER_TASK_STACK_DEPTH (configMINIMAL_STACK_SIZE * 2)

/* Set the following definitions to 1 to include the API function, or zero
to exclude the API function. */
#define INCLUDE_vTaskPrioritySet 1
#define INCLUDE_uxTaskPriorityGet 1
#define INCLUDE_vTaskDelete 1
#define INCLUDE_vTaskCleanUpResources 1
#define INCLUDE_vTaskSuspend 1
#define INCLUDE_vTaskDelayUntil 1
#define INCLUDE_vTaskDelay 1
#define INCLUDE_xQueueGetMutexHolder 1
#define INCLUDE_xTaskGetSchedulerState 1
#define INCLUDE_eTaskGetState 1

/* Cortex-M specific definitions. */
#ifdef __NVIC_PRIO_BITS
/* __BVIC_PRIO_BITS will be specified when CMSIS is being used. */
#define configPRIO_BITS __NVIC_PRIO_BITS
#else
#define configPRIO_BITS 4 /* 15 priority levels */
#endif

/* The lowest interrupt priority that can be used in a call to a "set priority"
function. */
#define configLIBRARY_LOWEST_INTERRUPT_PRIORITY 0xf

/* The highest interrupt priority that can be used by any interrupt service
routine that makes calls to interrupt safe FreeRTOS API functions. DO NOT CALL
INTERRUPT SAFE FREERTOS API FUNCTIONS FROM ANY INTERRUPT THAT HAS A HIGHER
PRIORITY THAN THIS! (higher priorities are lower numeric values. */
#define configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY 5

/* Interrupt priorities used by the kernel port layer itself. These are generic
to all Cortex-M ports, and do not rely on any particular library functions. */
#define configKERNEL_INTERRUPT_PRIORITY (configLIBRARY_LOWEST_INTERRUPT_PRIORITY << (8 - configPRIO_BITS))
/* !!!! configMAX_SYSCALL_INTERRUPT_PRIORITY must not be set to zero !!!!
See http://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html. */
#define configMAX_SYSCALL_INTERRUPT_PRIORITY (configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY << (8 - configPRIO_BITS))

/* Normal assert() semantics without relying on the provision of an assert.h
header file. */
#define configASSERT(x) \
 if ((x) == 0) { \
 taskDISABLE_INTERRUPTS(); \
 for (;;); \
 }

/* Definitions that map the FreeRTOS port interrupt handlers to their CMSIS
 standard names. */
#define vPortSVCHandler SVC_Handler
#define xPortPendSVHandler PendSV_Handler

/* IMPORTANT: This define MUST be commented when used with STM32Cube firmware,
 to prevent overwriting SysTick_Handler defined within STM32Cube HAL */
/* #define xPortSysTickHandler SysTick_Handler */

#endif /* FREERTOS_CONFIG_H */

 

I've tried with plain FreeRTOS and CMSIS v2, but none of them are executing the task.

I would appreciate ideas of where the errof might be comming from. I've thought of an error in my FreeRTOS config, or a misconfig in the clocks, but my project worked with only hal

I can share more of the code, if necessary

This topic has been closed for replies.

5 replies

mƎALLEm
ST Technical Moderator
November 4, 2024

Hello @laplaga and welcome to the community.

Not sufficient as info.

You need to share your main and the task.

Did you try to toggle your LED without RTOS? it could be something wrong with the GPIO config.

You didn't tell which board are you using ST or custom board?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
laplagaAuthor
Associate
November 4, 2024

Thanks, I've tried to toggle them without RTOS, and it worked, so I'm pretty sure that is not the problem :)

I'm using the STM32F303RE nucleo board

 

 

The main is here:

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

#include "gpio.h"
#include "tim.h"
#include "usart.h"

/* FreeRTOS includes. */
#include <FreeRTOS.h>
// #include <queue.h>
// #include <semphr.h>
#include <task.h>
// #include <timers.h>
// CMSIS Include
#include "cmsis_os2.h"

/* Standard includes. */
#include <stdio.h>

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */

/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */

/*-----------------------------------------------------------*/
osThreadId_t defaultTaskHandle;
const osThreadAttr_t defaultTask_attributes = {
 .name = "BlinkyThread",
 .stack_size = 128 * 4,
 .priority = (osPriority_t)osPriorityNormal,
};
void BlinkyThread(void* argument);
/*-----------------------------------------------------------*/
void BlinkyThread(void* argument) {
 HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
 while (1) {
 HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin); // Toggle LED (adjust pin as necessary)
 osDelay(500); // Delay for 500 milliseconds
 }
}

// static void exampleTask(void* parameters) __attribute__((noreturn));
// static void exampleTask(void* parameters) {
// /* Unused parameters. */
// (void)parameters;

// HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);

// for (;;) {
// /* Example Task Code */
// HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
// vTaskDelay(100); /* delay 100 ticks */
// }
// }

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void) {
 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_TIM1_Init();
 MX_TIM2_Init();
 MX_TIM3_Init();
 MX_TIM4_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 osKernelInitialize();

 // Create the Blinky thread
 defaultTaskHandle = osThreadNew(BlinkyThread, NULL, &defaultTask_attributes);

 // Start the RTOS kernel
 osKernelStart();

 // This is a fake comment, delete
 for (;;) {
 /* Should not reach here. */
 }

 return 0;
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void) {
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) {
 Error_Handler();
 }
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void) {
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1) {
 }
 /* USER CODE END Error_Handler_Debug */
}

#if (configCHECK_FOR_STACK_OVERFLOW > 0)

void vApplicationStackOverflowHook(TaskHandle_t xTask, char* pcTaskName) {
 /* Check pcTaskName for the name of the offending task,
 * or pxCurrentTCB if pcTaskName has itself been corrupted. */
 (void)xTask;
 (void)pcTaskName;
}

#endif /* #if ( configCHECK_FOR_STACK_OVERFLOW > 0 ) */

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t* file, uint32_t line) {
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

mƎALLEm
ST Technical Moderator
November 4, 2024

Could you please share your project including your ioc file?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.