User Activity

Hello.I have some issues with creating working project in STM32Cube.Creator asks for this:Also I read this:https://community.st.com/t5/stm32-mcus/stm32cubeide-how-to-debug-an-stm32h7rx-sx-project-without/ta-p/737120This indicates that there are two s...
HelloCan anybody explain how it is possible to power VCORE directly from SMPS output? I see that SMPS have only two possible output voltages, 1.8V and 2.5V:But VCORE accepts absolute maximum of 1.4V.So how it is possible with LDO bypassed?Best Regard...
Hi.In X-CUBE-USB-AUDIO, You wrote:1. Does it mean that playback and recording can work simultaneously, and at different sampling rates? For example, playback at 44,1k, and recording at 96k?2. Does it mean that playback and recording may by governed b...
What exactly "MSL3 preconditioning" means?Does it mean the same as "baking"?This preconditioning corresponds with soldering, or all the time?How accuracy are affected by moisture?I understand that omitting the baking before soldering, will cause crac...
Posted on May 08, 2017 at 12:56Hi.So, main page says:So it suggest that STM32F7x8 and 7x9 has DSI, and lowest (7x2 to 7x7) doesn't.Unfortunately if we enter a specific type of microcontroller, exampleSTM32F777BI, we see general information about all...