STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB OTG Dual Role

Hi STM Team, I am using STM32H723ZGT6 Microcontroller for my new project, I am using Azure RTOS for My application.I required to copy my data to Pendrive (I am using USB Host Only Mode and USBX and FileX).As well as i also required to use USB CDC ACM...

rkuma.21 by Associate III
  • 1126 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L433 CAN filtering using mask mode

Hello, I am currently using a STM32l433 with the following configuration: CAN_FilterTypeDef CAN_FilterInitStructure = {0}; CAN_FilterInitStructure.FilterBank = filterNum; CAN_FilterInitStructure.FilterScale = CAN_FILTERSCALE_...

agennart_0-1744871209560.png
agennart by Associate II
  • 3981 Views
  • 10 replies
  • 0 kudos

Changing HSE and LSE source when CSS

Hello all,We are currently using the STM32G0B1RE in our design, where both HSE and LSE external oscillators are used. The PLL is configured to multiply the 8 MHz input to 64 MHz. All clock configurations are performed via STM32CubeIDE and HAL, and th...

Wadeva by Associate III
  • 1353 Views
  • 1 replies
  • 0 kudos

I2S Microphone Output Problems

Hello,I am a beginner trying to create my first STM32 project using the STM32F407G Discovery Board. I am trying to receive audio input through I2S, delay one of the channels, and then output the result to the audio jack. I can get a simple sine wave ...

Resolved! USBX Standalone example for CDC_ACM

Hi,I am implementing CDC ACM on STM32C0x series with USBX standalone. I searched for many examples but could not find a single example for USBX standalone for CDC ACM. There are examples with USBX standalone for HID Mouse. Wherever, I find example of...

PPate.1 by Associate III
  • 2913 Views
  • 4 replies
  • 3 kudos