STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Count External Clock pulses

Hi Team, Currently I am working with STM32U575ZiTx SOC and I am using Tim3 for counting external clock pulses, Can you guide me with the code please. Below is my requirement :  1. What is the maximum frequency of the incoming signal? (To ensure the t...

ram_jan by Associate II
  • 3552 Views
  • 10 replies
  • 0 kudos

stm32 custom bootloader

"I am currently developing a custom bootloader for the STM32F072RBT6 microcontroller. The bootloader is functioning correctly in terms of receiving via UART and writing application code of varying sizes into flash memory . I have verified the correct...

USBX on STM32C0 incomplete?

Hi All,I have previously experiemented with USB HID mouse coding on STM32F0 series and got code working very quickly.However, I am now trying to get the same going using USBX on STM32C0. My application has been built in MX but wouldn't enumerate. I a...

USB : TinyUSB for WebUSB

Dear community,i'm trying to use tinysub for WebUSB application.My device is already see as a HID device....In copy, my USB_descriptor.c  #include "tusb.h" #include "usb_descriptors.h" #include <string.h> // Identifiants USB #define USB_VID ...

JL_Loyd by Associate II
  • 2124 Views
  • 2 replies
  • 0 kudos

Resolved! How do I put the original flash bootloader back onto a device if I've erased or corrupted it?

I'm not sure how I did it, but my Blue Pill STM32F103C8T6 doesn't respond to st-info --probe any more. This has happened twice in a row with identical devices. It seems that if I Ctrl-D out of GDB (an old bad habit) the device seems to brick itself a...