STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Non blocking debug messages to UART

Hi, I'm using STM32H755 nucleo board. I'm running FREERTOS on core M7 and bare metal on M4. I have been sending debug messages through USART3. It has been working ok, but sometimes messages from different tasks are overlapping. I want to change code ...

mosamasa by Associate II
  • 1461 Views
  • 4 replies
  • 1 kudos

Resolved! STM UDP freezes for 20 seconds

TLDR; STM32Ethernet has udp problems where it freezes for 20 seconds after sending data for 20 seconds and 60 seconds. After this it runs smoothly. However i'd like for it to not freeze twice as it is important the data gets sent asap.Hi, i am using ...

Resolved! STM32H573: Ethernet - HAL_ETH_Init returns error.

I am using STM32H573 and trying to enable ethernet. I have used the below article for it:https://community.st.com/t5/stm32-mcus/how-to-use-the-lwip-ethernet-middleware-on-the-stm32h5-series/ta-p/691100But ethernet is not being initialized. The HAL_ET...

jowakar122_0-1747656677963.png

STM32G491 IAP

Hi,I'm working on firmware upgrade functionality for an STM32G491 series MCU. In our system, the MCU communicates with a processor over I2C, where the processor acts as the master and the MCU as the slave. Currently, we're using I2C1 on the MCU for t...

STM32 SDIO SD card initialization

Hi,I have an STM32F7 design with SD card connected via SDIO interface.In many posts I read that SD cards have to be initialized with a 1 bit wide bus and a clock of 400 kHz. Switching the bus width from 1 to 4 bit using the command HAL_SD_ConfigWideB...

JBurg.5 by Associate II
  • 1187 Views
  • 1 replies
  • 0 kudos

Resolved! Ethernet Speed is not sufficient in STM32F767

Presently we are using STM32F767ZI for our ongoing projects. Our application demands high speed data transfer rate through ethernet. We are taking the help of UDP for transfer of real time audio data between 2 STM32F767ZI Nucleo Boards. Further we ne...

vbk22398 by Senior
  • 6021 Views
  • 17 replies
  • 15 kudos

CMSIS only project for STM32F0

How do I get a non-HAL project going but with CMSIS for a STM32F051? I've seen a few references describing how to add various folders containing the required files to the projects build settings. The problem for me is the folders described do not exi...

U_db by Associate
  • 1146 Views
  • 1 replies
  • 1 kudos

Resolved! Issue with HAL_Delay() and ThreadX

Hello everyone,I am encountering an issue with the HAL_Delay() function and ThreadX in my project. Before initializing ThreadX, HAL_Delay() works as expected. Specifically, the callback function:void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *h...

JonConesa by Associate III
  • 1825 Views
  • 3 replies
  • 1 kudos