STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L152 UART code missing in driver

Good Day, Recently I started working with a new MCU (STM32L152). I ported some UART code to handle received data from a different MCU, which worked fine. But as soon as I started testing edge cases I saw some weird things happen. I am using the DMA o...

Resolved! RS485 DE enable

Hi,I am implementing RS-485 communication on the STM32G491. Based on available references, I’m currently using a custom GPIO pin for the DE (Driver Enable) signal, since the default USART1_DE pin is already allocated for another function. In the RS-4...

Resolved! STM32N657X0 with Classic USB device middleware

I am trying to add the NUCLEO-N657X0-Q (MB194-N657X0Q-C01) to the IMBootloader project, which currently uses the Legacy Classic USB device middleware. I ran into a problem where, after calling the HAL_PCD_Start() function, I receive an unexpected int...

IgorMisic_0-1749049890954.png
IgorMisic by Associate II
  • 1168 Views
  • 1 replies
  • 0 kudos

Resolved! Can't make Ethernet work for STM32H757I-EVAL

Hello,I followed https://community.st.com/t5/stm32-mcus/how-to-create-a-project-for-stm32h7-with-ethernet-and-lwip-stack/ta-p/49308 tutorial from the scratch to the end, including the Hello UDP part, and adding the "ETH CODE" code.However, I can't pi...

Matteo-uC by Associate III
  • 5189 Views
  • 24 replies
  • 6 kudos