Hi there,just found out, that there's a severe bug in STM32Cube_FW_H7_V1.11.2, file stm32h7xx_hal_ospi.c at line 1599 (Function HAL_OSPI_Receive_DMA), which prevents the OSPI DMA Receive mode from working correctly: /* Enable the transmit MD...
I'm operating an Infineon F-RAM CY15B116QSN at the OctoSPI port of an STM32H735 MCU with 100 MHz clock (F-RAM devices is specified up to 108MHz). The F-RAM datasheet requires a CS high time between commands of at least 145 ns, which requires 15 clock...