STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LL_RCC_PLL_ConfigDomain_XXX functions

Can anybody explain me what it the sense of having such functions separate for any peripheral that can choose the PLL as the source clock ?I mean... There is no independent "domains" for SYSCLK, ADC, I2S, etc.... There is only one instance of PLL and...

Resolved! Ethernet issue on NUCLEO-H723ZG

Hi. I have a NUCLEO-H723ZG board. And my basic goal is to create from scratch non-rtos project with ethernet support. But after many attempts i cant get it respond to pings from PC. I tried flashing udp echo sample and it works, so hardware isnt faul...

AlexCatze_0-1747475977037.png AlexCatze_1-1747476047272.png AlexCatze_2-1747476200315.png AlexCatze_3-1747476220359.png
AlexCatze by Associate II
  • 2634 Views
  • 6 replies
  • 3 kudos

STM32H745 PTP Offloading

HelloI’m busy with the implementation of PTP support inside my project.I choose the STM32H745, because there is PTP support in hardware, with a nice offload function. After reading and try to understand the manual I create this code:uint32_t SubSecon...

JDWBE by Associate III
  • 4188 Views
  • 18 replies
  • 2 kudos

STM32H743 ETH DMA MPU SETTING

 Hello everyone, I am using the LWIP protocol stack on an STM32H743.I'm a bit confused about the MPU configuration here.I currently have the DMA receive and transmit descriptor addresses set to 0x30040000 and 0x30040100 respectively.The DMA receive b...

LL Driver Support for SPI on STM32H743ZI

I am working on a project using the STM32H743ZI microcontroller.I want to implement SPI communication using the LL (Low-Layer) drivers instead of HAL. :question_mark: Can you confirm whether the STM32H743ZI supports LL SPI driver APIs like LL_SPI_Ini...

mohitha by Associate II
  • 2954 Views
  • 10 replies
  • 8 kudos

Creating new Project with X-CUBE-AUDIO-KIT

I am working on an audio application which is to be built on a custom board using STM32H723VG and the X-CUBE-AUDIO-KIT V1.1.1.  I have demonstrated a prototype solution using the pre-built AUDIO-KIT binary loaded on the STM32H735G-DK development boar...

JRies by Associate
  • 1452 Views
  • 2 replies
  • 0 kudos

Resolved! Systick sync with TIM3

I configured STM32CubeMX to have a timebase source as SysTick. I'm using this for my scheduler. its running at 1ms. I also configured tim3 for 1ms sortof.But for some reason this will not stay in synch with systick. They are drifting constantly apart...

Carl_G_0-1750822395221.png Carl_G_1-1750822499426.png
Carl_G by Senior III
  • 1389 Views
  • 9 replies
  • 3 kudos