cancel
Showing results for 
Search instead for 
Did you mean: 

SVD errors on STM32H503

hijax_pl
Associate III

Using python I have written small app to convert SVD V1.4 into assembly include. Then I started to write assemby code using RM0492 Rev2 .

For the peripherals I use (RCC,ADC,GPIO,GPDMA,TIM,USART) I have found that there are few errors in the SVD file, some typos etc.

Namely:

RCC_CCIPR5 register has only 2 fields described, no info about FDCANSEL, DACSEL & ADCDACSEL

RCC_CFGR regsiter shall be named RCC_CFGR1

For RCC_PLL1CFGR & RCC_PLL2CFGR there are DIVMx while should be PLLxM

 

 

 

4 REPLIES 4
STTwo-32
ST Employee

Hello @hijax_pl 

Thank you for reporting those typos. I'm escalating the second and the third points as they are for correction (under internal ticket number 197881). But the first point, I find that we have a typo only on the name and description of the bit values for DACSEL. They others looks fine on my side.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Yes, my mistake.

I have filtered out DAC & FDCAN as peripherals but also from RCC defines.

And yes, DACSEL is DAC1SEL in reference manual.

 

 

Do not know if I shall open new thread but anyway.

(1) Why TIM1_SMCR and TIM2/3_SMCR have different naming convetions for SMS / TS fields?

i.e. for TIM1_SMCR there are SMS/SMS_1 and TS/TS_1 and for TIM2/3_SMCR, SMS1/SMS2 and TS1/TS2 respectively.

(2) Also TIM1_SMCR_TS_1 field has no enumerated values, while for TIM2/3_SMCR_TS2 there are, but wrongly described. TIM1_SMCR_TS & TIM2/3_SMCR_TS1 has enums for the range 0..7 only, ie. the TS1 field itself.

As in the RM those fields must be combined, I think the easies way forward would be to provide enums only for the TS1 field, and add missing values:

B_0x10000:Internal Trigger 4 (tim_itr4)
B_0x10001:Internal Trigger 5 (tim_itr5)
B_0x10002:Internal Trigger 6 (tim_itr6)
B_0x10003:Internal Trigger 7 (tim_itr7)
B_0x10004:Internal Trigger 8 (tim_itr8)
B_0x10005:Internal Trigger 9 (tim_itr9)
B_0x10006:Internal Trigger 10 (tim_itr10)
B_0x10007: Internal trigger 11 (tim_itr11)
B_0x20000: Internal trigger 12 (tim_itr12)
B_0x20001: Internal trigger 13 (tim_itr13)
B_0x20002: Internal trigger 14 (tim_itr14)
B_0x20003: Internal trigger 15 (tim_itr15)

(and repeat that pattern for all other fields that are splitted acrose registers)

Then one can code by just shifting the chosen enum to the TS1 field position.

And this time: ADC_CFGR register and EXTSEL field.

In SVD this single field is split among four 1-bit long ones (according to RM0492) and enumerated values desciptions are messed up (adc_ext_trg0 & adc_ext_trg1 repeated for all 4 "subfields")

RM0492 discusses this as single field, which is correct, i.e.

"Bits 9:5 EXTSEL[4:0]: External trigger selection for regular group

These bits select the external event used to trigger the start of conversion of a regular group:
00000: adc_ext_trg0
00001: adc_ext_trg1
00010: adc_ext_trg2
00011: adc_ext_trg3
00100: adc_ext_trg4
00101: adc_ext_trg5
00110: adc_ext_trg6
00111: adc_ext_trg7
...
11111: adc_ext_trg31"

etc...

Is SVD created from RM or vice versa? Either way I think both RM0492 (page 579) and SVD shall be corrected.