STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F411, STM32CubeMX, USB Device for CDC

Posted on November 26, 2014 at 08:09STM32F411RCTx, LQFP64When using STM32CubeMX Ver4.4 to generate USB Device only code for CDC class, initialization is fine but cannot connect to PC (host).The STM32CubeMX generated code also has same problem as MDK...

bardeen by Associate
  • 1596 Views
  • 2 replies
  • 0 kudos

stm32f207 usb only multiple of 64 bytes can be send

Posted on April 10, 2013 at 10:04change by stm32 usb device VCP example: my send function: uint16_t VCP_DataTx (uint8_t* Buf, uint32_t Len) {  uint8_t i;  for (i=0;i<64;i++)    //only multiple of 64 bytes can be send   {  APP_Rx_Buffer[APP_Rx_ptr_in...

easylwl by Associate II
  • 3347 Views
  • 7 replies
  • 0 kudos

USB HS Host Unconfigures Device

Posted on March 20, 2014 at 21:13Was hoping there might be a few folks here with more USB knowledge than me. I am trying to implement a HS USB HID-class device on a STM32F427 using a SMSC USB3300 external PHY IC. I have succesfully implemented a si...

jvavra by Associate III
  • 1526 Views
  • 3 replies
  • 0 kudos

Stm32f427 system memory bootloader

Posted on November 29, 2014 at 12:54 i have custom board with STM32F427VI and want to boot from usart3 via bootloader inside system memory. boot0 pin is low and boot1 pin is NC. i dont want to switch boot pins. because eventually these pi...

0690X00000602z0QAA.jpg

Complete USB OTG power solution design

Posted on November 28, 2014 at 10:03Hi, I have been working on a power design that integrates with the STM32F401 utilizing OTG.  I would like to support OTG both as a host and device.  In addition, I would like to detect dedicated charging ports and...

Use STM32CubeF4 or Standard Peripherals or DIY?

Posted on November 26, 2014 at 02:01I can see that STM32Cube is the new hotness, but...I am starting a new project with the STM32F405xx and FreeRTOS (ideally the current rev 8.1.2).  It seems that there are lots of layers added to peripheral access ...

mduffy by Associate II
  • 948 Views
  • 2 replies
  • 0 kudos

STM32CubeF4 LTDC minor issues

Posted on November 16, 2014 at 16:37- In a comment in stm32f4xx_hal_ltdc.c   HAL_LTDC_ProgramLineInterrupt() is mentioned...but couldn't find such a function. It's not even declared in ''...ltdc.h''. - In the source of HAL_LTDC_ConfigCLUT function...

Examples of Custom USB Classes?

Posted on August 27, 2013 at 04:16I'm trying to code an app that communicates using USB bulk transfers but is simpler than the CDC/VCP and MSC examples in ST's library. I've tried to code a custom USB class, but Windows doesn't like it - it sends me...

mattscar by Associate II
  • 1735 Views
  • 2 replies
  • 0 kudos