STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube and FreeRTOS 8.1.2

Posted on November 18, 2014 at 05:28Any ETA for a version of STM32Cube that includes the latest version of FreeRTOS?Current version of http://www.freertos.orgis 8.1.2, but STM32Cube contains Version 7.6. #freertos-stm32cube

mduffy by Associate II
  • 2318 Views
  • 4 replies
  • 0 kudos

STM32 USB HS Performance

Posted on September 19, 2014 at 18:31I am thinking of using an external ULPI phy with the STM32F4. I will write a custom driver that would send and receive data using bulk end points. Assuming there is no bottleneck anywhere else on the system, what...

Using STM32F429I-Discovery as USB OTG MSC

Posted on July 25, 2014 at 18:29HiMy company wants to evaluate the STM32F429I-Discovery kit and its functions.One of the applications I have to develop will consist in using the board itself as a USB OTG Mass Storage Class, so that I can transfer fi...

michel by Associate II
  • 6830 Views
  • 14 replies
  • 0 kudos

USB Lib STSW-STM32121; V4.0.0 bug report

Posted on November 14, 2014 at 20:26In usb_regs.h wrong bits are assigned for register OTG_FS_DOEPCTL0 or OTG_HS_DOEPCTL0 to the structer typedef union _USB_OTG_DEPCTL_TypeDef. Althought the names of bits are ok, their position doesn't match with wi...

STMF4Discovery - FatFS write nonsense

Posted on November 11, 2014 at 11:34Hi,I'm testing FatFS with STMF4Discovery board and I have issue when I write some bytes sequnce. Generally FatFS works well, reading, writing, format, but  when I try to write data sequence: '0xAEAE' I get the wro...

vukasheen by Associate II
  • 1349 Views
  • 3 replies
  • 0 kudos