cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with clock configuration of NUCLEO-L152RE using STM32Cube

angelo2
Associate
Posted on November 21, 2014 at 16:00

Hello, I'll be glad to recibe any help.

I've created a project for the NUCLEO-L152RE using STM32Cube (selecting the correct board) and then I've exported it to IAR-EWARM. When I run the project into the board, the MCU don't continue after the clock configuration. If I go step by step over the code, when the HSI clock is set, all stops.

The configuration clock option was: HSI RC (16MHz) --> PLLCLK (x4 /2) --> SYSCLK (32MHz). All the other configurations by default.

I'll appreciate any help! Thanks! 

#nucleo-l152re #stm32cube
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
juergen2399
Associate
Posted on November 25, 2014 at 14:12

Hi,

do you have external clock connected to the L152RE?

By default there is no oscillator nor is there a connection to ST-LINK-clock 'MSO' and the controller can run only with internal clock.

See Nucleo User Manual UM1724 ('STM32 Nucleo boards' -

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00105823.pdf)

- chapter 5.7 for clock supply options.

BR

Jürgen