STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trouble Using Input Capture with HAL Library

Posted on September 20, 2016 at 19:00Hello everyone,A week's search didn't bring me very far, so I thought I should ask You guys. I have some experience using Arduino, but this is my first hard-core microcontroller project and so far the learning cu...

Logging data to USB

Posted on September 16, 2016 at 16:54Hello to everyone,I am developing an application that reads data from sensors mounted on a STM32L4 discovery board, but since I need to log for hours I need to save data on a big storage support, such as an USB.I...

Ethernet lwip on STM32F407 board with HAL lib.

Posted on June 08, 2016 at 12:25 Hello. I want to make an UDP communication using mySTM32F407 based board, where the PC forms the server side. I checked most of the posts related to the Ethernet+F407 topic, but could not find any c...

0690X00000605OzQAI.png
akosodry by Associate II
  • 5981 Views
  • 7 replies
  • 0 kudos

STM32F427 CAN Error Status

Posted on September 15, 2016 at 17:40STM32CubeMX 4.16  STM32Cube FW_F4 V1.13.0 I have CAN working OK and need to get the Error Status, I have the following Code fragment but do not receive an Error Code when a CAN Error occurs i.e. disconnected.    ...

DISCO_F746NG - using BSP_AUDIO on mbed

Posted on November 30, 2015 at 17:09Hi all, I'm trying to get the BSP audio drivers working with the mbed Arm online compiler. ST has posted a numbed of the drivers for the new F7 discovery board https://developer.mbed.org/teams/ST/code/BSP_DISCO_F7...

bc by Associate II
  • 1460 Views
  • 2 replies
  • 0 kudos

CAN-Bus Problems

Posted on July 09, 2014 at 13:53Hi, Has anyone run a CAN application that works also in error cases? In my application the connection hangs, for example, after pulling the CAN bus pin plug and re-connect. One reason for this is the HAL_CAN_Transmit ...

STM32F103 series bootloader PC software.

Posted on July 01, 2011 at 06:00Hello All, I am new to STM32F103 MCUs. I know it can boot from system area containing a factory programmer ST bootloader that uses USART1 interface. So I thought there must be a ISP utility from ST can (like the Flash...