STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Composite Device Bug

 I have setup a Nucleo-F103RB as a USB composite device by (CDC + HID) by modifying a STM32CubeMX CDC project. The device enumerates correctly and everything works initially, however I am encountering a strange bug where if I open a COM port to read ...

Apisit-K by Associate
  • 927 Views
  • 2 replies
  • 0 kudos

zephyr stm32u073 usb

Hello,I am trying to get the USB HID working on STM32U073 with ZephyrOS.I took the sample code from https://github.com/zephyrproject-rtos/zephyr/tree/v4.2.0/samples/subsys/usb/hid-mouseAnd tried both the NEXT and legacy USB stack. However, when I boo...

pokitoz by Associate II
  • 749 Views
  • 1 replies
  • 1 kudos

Resolved! USB Composite Design (CDC+HID Keyboard)

Dear STM32 Advisor,   I'll design a system based on Nucleo 64 H533RE. The system will act as USB CDC and USB HID Keyboard at the same time. The idea is when the CDC receive a character, here for example "F" then the Nucleo H533RE will output a high g...

FuadPurnomo_0-1760197412665.png

Resolved! STM32H75x LwIP Flash Size Way Too Large

Hello, I am working to implement LwIP onto my MCU (STM32H750VBT6TR) with the PHY (DP83825IRMQR). I got everything set up and was able to do a ping test and create a basic UDP client to send and receive packets (see this thread). This works well on my...

CMHenway_0-1760033273251.png CMHenway_1-1760033297361.png
CMHenway by Associate II
  • 833 Views
  • 6 replies
  • 3 kudos

Resolved! How to use fx_media_format and fx_media_open ?

Hello,I am trying to set up FileX with USBX, but my computer recognizes a disk drive but does not see any volume.Can you help me determine whether I am using the fx_media_format and fx_media_open functions correctly, given that they do not return any...

RemiNao by Associate III
  • 749 Views
  • 1 replies
  • 1 kudos

Resolved! STM32H7 PTP NETXDUO

Hello, I would like to know if this PTP client example from Netxduo can be used on an STM32H723 MCU: https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/netx-duo/netx-duo-ptp-client/chapter1.md Another MCU, the STM32N6 has this implement...

FB__1 by Associate III
  • 2490 Views
  • 12 replies
  • 9 kudos