cancel
Showing results for 
Search instead for 
Did you mean: 

How to use fx_media_format and fx_media_open ?

RemiNao
Associate III

Hello,

I am trying to set up FileX with USBX, but my computer recognizes a disk drive but does not see any volume.
Can you help me determine whether I am using the fx_media_format and fx_media_open functions correctly, given that they do not return any errors?

 

  UINT ret = FX_SUCCESS;
  /* USER CODE BEGIN MX_FileX_Init */
  UINT RETT = lx_stm32_nor_custom_driver_initialize(&nor_flash);

  /* USER CODE END MX_FileX_Init */

  /* Initialize FileX.  */
  fx_system_initialize();

  /* USER CODE BEGIN MX_FileX_Init 1*/

  /* Format the NOR flash as FAT */
	  status =  fx_media_format(&nor_flash_disk,
	                            fx_stm32_levelx_nor_driver,   // Driver entry
	                            (VOID*)&nor_flash,            // Device info pointer  (VOID*)NOR_CUSTOM_DRIVER_ID
								(UCHAR*)media_memory,         // Media buffer pointer
	                            sizeof(media_memory),         // Media buffer size
	                            "NOR_FLASH_DISK",             // Volume Name
	                            1,                            // Number of FATs
	                            32,                           // Directory Entries
	                            0,                            // Hidden sectors
								TOTAL_SECTOR_LOGICAL,		  // Total sectors
								SECTOR_SIZE_LOGICAL,          // Sector size
	                            8,                            // Sectors per cluster
	                            1,                            // Heads
	                            1);                           // Sectors per track
  /* Check if the format status */
  if (status != FX_SUCCESS)
  {
    Error_Handler();
  }

  /* Open the SPI NOR Flash disk driver.  */
  //status =  fx_media_open(&nor_flash_disk, "FX_LX_NOR_DISK", fx_stm32_levelx_nor_driver,(VOID*)NOR_CUSTOM_DRIVER_ID , media_memory, sizeof(media_memory));
  status =  fx_media_open(&nor_flash_disk, "FX_LX_NOR_DISK", fx_stm32_levelx_nor_driver,(VOID*)NOR_CUSTOM_DRIVER_ID , media_buffer, sizeof(media_buffer));
  /* Check the media open status.  */
  if (status != FX_SUCCESS)
  {
    Error_Handler();
  }

 

For Device info pointer, should i use (VOID*)&nor_flash or (VOID*)NOR_CUSTOM_DRIVER_ID ?
Can the volume name and media name be different ?

 

1 ACCEPTED SOLUTION

Accepted Solutions
T_Hamdi
ST Employee

Hello @RemiNao 

You must use the same pointer (either (VOID)&nor_flash* or (VOID)NOR_CUSTOM_DRIVER_ID*) in both fx_media_format  and fx_media_open because the driver requires a consistent device context to properly access and manage the media. Using different pointers can result in the volume not being recognized correctly.

 

For Device info pointer, should i use (VOID*)&nor_flash or (VOID*)NOR_CUSTOM_DRIVER_ID ?

If you are using an official ST driver (such as LevelX for NOR QSPI), you should pass (VOID)NOR_CUSTOM_DRIVER_ID* because the driver uses this ID internally to manage the device. If you are using a custom driver or your own device management, you should pass (VOID)&nor_flash*, which is a pointer to the structure holding the hardware context. its correcte .

Can the volume name and media name be different ?

yes, the volume name and the media name can be different.


you can find a relevant example here to help you in your application here: 

ST FileX NOR Flash Write/Read Example 

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Hamdi Teyeb

View solution in original post

1 REPLY 1
T_Hamdi
ST Employee

Hello @RemiNao 

You must use the same pointer (either (VOID)&nor_flash* or (VOID)NOR_CUSTOM_DRIVER_ID*) in both fx_media_format  and fx_media_open because the driver requires a consistent device context to properly access and manage the media. Using different pointers can result in the volume not being recognized correctly.

 

For Device info pointer, should i use (VOID*)&nor_flash or (VOID*)NOR_CUSTOM_DRIVER_ID ?

If you are using an official ST driver (such as LevelX for NOR QSPI), you should pass (VOID)NOR_CUSTOM_DRIVER_ID* because the driver uses this ID internally to manage the device. If you are using a custom driver or your own device management, you should pass (VOID)&nor_flash*, which is a pointer to the structure holding the hardware context. its correcte .

Can the volume name and media name be different ?

yes, the volume name and the media name can be different.


you can find a relevant example here to help you in your application here: 

ST FileX NOR Flash Write/Read Example 

 

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Hamdi Teyeb