Hello,I am making a dev board for this new family of MCU, I need USB programming and power delivery.To make it I am referring to the datasheet, Nucleo dev board and to the application note.I did only once a board with STM32 and it was an F1. I can se...
Posted on December 26, 2017 at 12:40hello,I was wondering which is the policy of ST for the samples for students. I have been using free samples from AVR even before it was Microchip.If it is possible to ask for samples to ST which is the correct wa...
Posted on June 03, 2017 at 18:53hello,I would like to have some clarification about the USB circuit needed for the stm32f103 (and similar), I am making a simple development board just to start learning this MCUThis is taked from the maple mini https...
Posted on May 23, 2017 at 00:19 hello, I am working with this MCU for the first time, i used AVR until today, I would like to start with a minimum circuit to do some experimenting. I m using this schematics but i don't have any idea if is goo...
I just updated the question with a pic of the last schematics, as @TDK suggested.> 1) Pull up for DPI removed all the resistors on the DM/DP lines but I keept the two capacitors, should I remove also them?> 3) VREF pin usageI would do as you suggest...
Posted on June 28, 2018 at 11:28stm32duino is actually stm https://github.com/stm32duino see the 'people' box, the only one who doesn't work for stm is Roger, who was one of the first one to make a core for stm32 boards https://github.com/rogerclark...
Posted on February 24, 2018 at 15:43hello, like you i would like to start with stm32, I am still in the phase of gathering information around googlestm bought atollic so https://atollic.com/truestudio/ is now free and i think it would be a very goo...
Posted on January 06, 2018 at 10:28 Golab.Bogdan I already know about that tiny, cheap, wonderful board. I have been using it for more then a year I also know stm32duino good work to use the arduino environment which I used to make some little ...