STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using USB VID from ST

Hello all,We are planning to use the Murata CMWX1ZZABZ (STM32L072) for our low volume product. This entails the usage of the USB MSC library and therefore the usage of a VID and PID. We know that we can use the USB VID for evaluation purposes but is ...

TW.16 by Associate
  • 746 Views
  • 0 replies
  • 0 kudos

using stm32L151VE dual bank boot

I am using STM32L151VE. Trying to use the dual boot banks mechanism.I am compiling the code to 0x0 and load it to bank1 OR bank2 and setting the VTOR accordingly.When the code is located in bank1 and BFB2 is on - the application is running (memory ma...

MHirs by Associate
  • 1638 Views
  • 3 replies
  • 0 kudos

Using freeRTOS with lwip

I am currently trying to setup lwIP with freeRTOS using CubeMX. Using the generated code, creates a defaultTask, which initilializes the lwIP stack. It works just fine to ping the controller, but what i don't understand is, that in lwipopts.h NO_SYS ...

SoFa by Associate II
  • 744 Views
  • 0 replies
  • 0 kudos

PID sublicencing

Hello Sir, I am Vipul from Inceptor Technology Pvt. Ltd. Company is manufacturing Electronic Braille Display (BrailleMe) for visually challenge persons. We are using STM32H7 & STM32F1 Series controller in our device. Our Device communicates with win...

vkute by Associate
  • 977 Views
  • 1 replies
  • 1 kudos

Bug report for STM32F765

Hi,As part of SOUP (Software of Unknown Provenance) validation for a Class C medical device, i need to provide a couple of information.I am using STM32F7xx series of microcontroller (specifically STM32F765). The version number in use is V1.1.2, i und...