STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USB PD AVS support in X-CUBE-TCPP

Hello, I don't seam to see anything related to the implementation of the USB PD AVS system to allow a sink to request voltages of up to 48V. Am I miss-reading the X-CUBE-TCPP code? If it is missing, is there a plan to implement it? Thanks a lotHave a...

Resolved! Read temperature calibration value doesn't work

Dear SupportI am using STM32H563, try to get internal Vref, and temperature working, and ADC conversion is OK, but when using macro  __HAL_ADC_CALC_VREFANALOG_VOLTAGE, and __HAL_ADC_CALC_TEMPERATURE to convert to Vref and temperature, it ends up a in...

Ping1 by Associate II
  • 476 Views
  • 1 replies
  • 0 kudos