User Activity

Dear Community,I am working with an STM32F407 development board, using an ESP32 as a Wi-Fi modem controlled through AT commands. I am attempting to perform an MQTT test with AWS IoT using mbedTLS for the TLS handshake.I found the following mbedTLS im...
Hi everyone,I occasionally run into an error when flashing code to my board using the IDE. The error message is as follows: Failed to bind to port 61235, error code -1: No error Failure starting SWV server on TCP port: 61235 Failed to bind to por...
Title edited to reflect the correct board used. Changed from NUCLEO-H7A3ZI-Q to NUCLEO-H7S3L8.Hi,I’m trying to set up UART communication using UART3 on the NUCLEO-H7A3ZI-Q board. I have the UART3 pins (PD8 and PD9) connected to the ST-Link VCP on thi...
Hello ST Community,I have a question regarding the compatibility of the STLINK-V3MODS SWD pins with my MCU's SWD pins, which operate at 3.3V. Do I need to use logic level shifters between them, or are the STLINK-V3MODS SWD data signals fully compatib...
Hi everyone,I'm working with the STM32F429i-Disc1 board, writing code from scratch, and I encountered something odd. I created an empty project for the LCD, and during the LTDC pin initialization, I mistakenly set the alternate function (AF) to the w...
Kudos given to