Hello!i have followed your advise , i have instrumented with UART i found someting really strange to me: the problem occours in this piece of code (that work without problem in the main):uint8_t CSP_QUADSPI_Init(void){ uint8_t mark1[] = "MARK1";uint...
thank you for your advice!i will try the UART method (UART3 is connected to the st link on board)but if the problem is in the linker i think maybe the init function is not called from the cube programmer best reguards
thank you for your kind messagei have tried, i have modified the linker and the loader_Src.c fileunfortunately is not working, i will continue to tryi attache anyway the files to this message, maybe are useful for other peoplethe only modification th...
hello Tesla Deloreani have tried your loader and work fine! but i 'm trying to learn to make one.then i have tried to modify my project with your linker file but it doesn't workjust use your linker is not possible, it don't compile , Cube code need ...
Thank you for your message!i have a functioning driver for the memory, tested with the code attached (equal to the suggested code from the ST mooc) so i think the HW is correct, i think my problem is in the linker file or the Loader_Src.c filethank y...