STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Normal USB CDC Cannot Define after update.

I was used normal mode USB CDC with Host Only -> and in middleware ( USB CDC) And it worked no matter what and good for beginners. After Update That files ware missed with same settings-up for new project. i was in middle in middle of the project for...

Laksahan by Associate
  • 729 Views
  • 1 replies
  • 0 kudos

STM32 USB CDC not working for F0, F4 boards

I have tried USB examples for Stm32F070, F401, F407 Black board and calling a single "CDC_Transmit_FS" function to print a string but none is working. The hcdc->TxState value is some garbage big value so it always stay busy and also not getting inter...

Lakshay by Associate
  • 647 Views
  • 1 replies
  • 0 kudos

Resolved! CMSIS-DSP rfft init throwing an error

STM32WB55arm_rfft_fast_instance_f32 fft_instance; arm_rfft_fast_init_f32(&fft_instance, NUM_SAMP);I'm trying to use the rfft_fast function from the arm_math.h libraryBut when I compile I get... ../STM32_WPAN/App/custom_app.c:122:24: error: expected d...

Resolved! STM32F446 - SPI DMA

What's wrong with my code? Every time I start a DMA transfer only 2 Bytes get transferred although I specified 16 bytes.Also, I get an FIFO Error after transmit, whereas Transmit Complete is ok./* FUNCTION ************************************/ void S...