STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_Delay works and doesn't work

I'm still very new to STM32 processors, and using CubeMX to generate my basic code structure (for TrueStudio). In the code below, if I uncomment code section A, the yellow LED blinks, but not evenly... At low values such HAL_Delay(100), the high time...

NNar by Associate II
  • 3421 Views
  • 4 replies
  • 0 kudos

stm32h743 lwip HOSTNAME trouble

I am new to stm32h743. I have ported project LwIP_TCP_Echo_Server for eval pcb to nucleo h743 and all works ok. Within the dhcp list of linked device see my device with "unknown" name. I have added "#define LWIP_NETIF_HOSTNAME 1" into the lwipopts.h ...

EBrun by Associate II
  • 825 Views
  • 0 replies
  • 0 kudos

STM32 not working when leave USB or dont plug USB

Hi guys,I have a program use USB CDC and some function(STM32F103C8T6 StdPeriph lib). If use USB to power supply then program normal working, but it's working I leave USB out from Board (have sub power supply for Board) Program stop now. And if don't ...

TPham.10 by Associate II
  • 1666 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L0 use internal EEPROM

Hello,i just want to use the Internal EEPROM of my STM32L052.I followed the short description in the STM32CubeMX manual. But it is not working. Here my small code example HAL_FLASHEx_DATAEEPROM_Unlock(); HAL_FLASHEx_DATAEEPROM_Erase(0x08080000U); ...

Why STM32H743ZI DFU bootloader does not come up?

Hell ST community!I have made a board with an STM32H743ZI MCU on it. It has connections to pins where serveral USART peripherals sit (without pull-ups) and uses USB FS on PA9 to PA12.My problem is that the DFU bootloader does not show up via USB. If ...

martin.k by Associate II
  • 4503 Views
  • 8 replies
  • 0 kudos

Resolved! Canbus Filter Matching Index

Hi, I'm fairly new to arm platform. I'm trying to communicate between 2 MCU via Canbus. with the latest HAL Library I set up 4 filters (2 for each fifo) id mask type , 32Bit. I am receiving my messages from correct fifos. what I cant get is filter ...

e-zeki by Associate III
  • 5293 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.