STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, I try to upload my STM32 F446RE using bootloader through CAN. I get the STLINK V3SET and the utility STM32CuebeProgrammer. But the connection with the target is impossible.

I get few questionning:The STLINK does not detect any target voltage on the T_CAN_VCC pin, whereas I put 3.3V from my STM32 on it. What can I do ?The documentation says to put BOOT0 high and BOOT1 low. that's what I did. But connection's still imposs...

Zephyr S by Associate II
  • 826 Views
  • 0 replies
  • 0 kudos

Resolved! Fatfs create folders

Hi All,I am currently working on creating a file system on an stm32f207, using the nucleo board for the time being while I wait for my custom boards.The board will have an SD card as well as a USB. I have made a simple function for creating a folder ...

stm32h7 nucleo clock setting

I use stm32h7 nucleo board and there is gpio example in stm32cubeh7 and I changed clock configuration ,but it doesn't work.STM32CUBEh7-project-nucleo-example-gpio-gpio extstatic void SystemClock_Config(void) { __IO uint32_t StartUpCounter = 0, HS...

Bilge by Associate III
  • 990 Views
  • 0 replies
  • 0 kudos

FreeRTOS +LwIP + FreeModbus TCP Hanging

I am using STM32F746ZG Nucleo board and programmed Modbus TCP with FreeRTOS(LwIP). Initially boad report properly to Modbus Master simulator, after ~10 hours or above any time, MCU going infinite loop some exception function like hardware fault etc, ...

PNata by Associate II
  • 2483 Views
  • 4 replies
  • 0 kudos

Resolved! May have a bug in STM32Cube_FW_F7

Hello,In STM32Cube_FW_F7 for STM32F769I_EVAL Board, in sample for IAP_Main, in this directory:"STM32Cube_FW_F7_V1.X.X\Projects\STM32F769I_EVAL\Applications\IAP\IAP_Main\Inc\flash_if.h"in line 94 i saw the address of Sector 11 is wrong. It is Curren...

Slh by Senior
  • 1100 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.