STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Is there I2C Bootloader on STM32L051K8?

I am using STM32L051K8 MCU in my project. All the project has been developed. Now there is a need to provide OTA firmware upload. For that I require to use I2C bootloader as I have alreadey interfaced I2C EEPROM. Please let me know whether it is poss...

AJadh.5 by Associate
  • 2001 Views
  • 3 replies
  • 0 kudos

Resolved! BSP example of 32L476GDISCOVERY

Hi,I am working on board STM32L476G-DISCO, and I want build the example in STM32Cube_FW_L4_V1.13.0 Repository, ({USERNAME}\STM32Cube\Repository\STM32Cube_FW_L4_V1.13.0\Projects\32L476GDISCOVERY\Examples\BSP),it all build successfully but at the end i...

RKhal.2 by Associate III
  • 1964 Views
  • 2 replies
  • 2 kudos

STM32F469 VDDUSB when using external USB ULPI PHY

Hi,We're using an STM32F469NI in combination with an external ULPI PHY for HS-USB. All is working good but I have a question about VDDUSB. We connected it to 3.3V as we thought we needed to do when using any USB functionality but we didn't realise th...

eamonn2 by Associate II
  • 2619 Views
  • 5 replies
  • 0 kudos

USB Host HID problem with keyboards

Hi Im using stm32f4 discovery board to initial keyboard but when i connect the keyboard to board it detects the keyboard but didnt send any information.I change the keyboard and use microsoft curve keyboard 3000 and nothing changedIm using STM32CUBE...

AAgha by Associate II
  • 1979 Views
  • 3 replies
  • 0 kudos

Bug HAL_delay() off by 1ms

By coincidence I discovered a bug in HAL_delay(). __weak void HAL_Delay(uint32_t Delay){ uint32_t tickstart = HAL_GetTick(); uint32_t wait = Delay; /* Add a period to guaranty minimum wait */ if (wait < HAL_MAX_DELAY) {   wait++; } while((HAL_GetTick...

Lama by Associate III
  • 3499 Views
  • 9 replies
  • 0 kudos

STM32Cube FW-F4 V1.21.0 Uart Driver Bug

I'm using STM32 Cube FW-F4 V1.21.0 to generate UART driver code, it seem has a bug for:HAL_UART_Transmit_IT(UART_HandleTypeDef*huart, uint8_t *pData, uint16_t Size).The UART will not send thepacket if any data in *pData = 0. For example:HAL_UART_Tran...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.