STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeF1 software Patch

Dear Sir.​I downloaded Patch_STM32CubeF1 on the web of ST. However, it was decompressed but it was in version "STM32Cube_FW_F1_V1.6.0". On WEB is "1.7.1" Does anyone know any patch file of the correct version?

HUmet by Associate
  • 730 Views
  • 2 replies
  • 0 kudos

FatFs in STMCUBE

Hi,I have tested the FatFs on the STM32Cubemx,I have tested it on two different MCU's, STM32F401RC and STM32F429IGT6, it only works in the 1Bit mode on the STMF429 part, But the same settings on the STMCUBE and the STM32F401RCT6 part would not work, ...

stm32f207 composite USB device

Posted on July 25, 2013 at 09:37I'm trying to create a composite full speed device which combines HID (vendor specific) and Mass Storage.Anybody out there managed to create a working composite device using the ST libraries for the f2xx? (or f4xx)The...

adrian by Associate III
  • 1511 Views
  • 7 replies
  • 0 kudos

USB Host Audio Class- how to handle

Hello,Is there any working example of USB Host Audio Class? I am trying to run it using the API but I am having some hard time. In repository there is no example (in any repository) and there are no user manuals.I am able to connect to the USB Audio ...

maciek by Associate II
  • 862 Views
  • 1 replies
  • 0 kudos

Freertos and HAL external interrupts

Posted on November 09, 2017 at 15:39Hello,I'm using stm32l496.i'm trying to control LEDs with pwm through freeRTOS and using external Interrupts (gpio buttons)i have some questions :  i have some tasks looping while(1) to detect my input GPIO  and l...