cancel
Showing results for 
Search instead for 
Did you mean: 

USB Host Audio Class- how to handle

maciek
Associate II

Hello,

Is there any working example of USB Host Audio Class? I am trying to run it using the API but I am having some hard time. In repository there is no example (in any repository) and there are no user manuals.

I am able to connect to the USB Audio Device (USB Audio adapter). but when it somes to actual "playing" I can not make any resonable music. I can only make some "random" sounds. I am reading data from SD card and feeding it to USB. Everything works with I2S and audio codec so the data is not corrupted.

Do you guys have any github projects or something that worked?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hi @maciek​ ,

You find an Audio example under STM32Cube_FW_F4_V1.23.0\Projects\STM324xG_EVAL\Applications\USB_Host\AUDIO_Standalone for example.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.