STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F7-FFS-FreeRTOS Hard Fault

I am working with a sample project for the stm32F746G. Testing on the Discovery Board. I am using VisualGDB. The project is USB Device | MSC Host RTOS. After importing the project and tweaking a few things It did run. (However, all of these projects ...

Jona by Associate III
  • 635 Views
  • 1 replies
  • 0 kudos

Resolved! Issue with X-NUCLEO-IDW04A1

Posted on April 13, 2018 at 01:22Hi,I recently bought the following development boards : - NUCLEO-L476RG- X-NUCLEO-IDW04A1 (Wifi expansion board)I am also using the following software packages: - STM32Cube_FW_L4_V1.11.0- STM32CubeExpansion_WIFI1_V3....

ST DFU Bootloader Issue with some USB ports

Hi community, I implemented a C# application to monitor, configure and upgrade a ST device (STM32F072). On my development notebook it works fine, but only if I connect the device via USB with the docking station or to my laptop without docking statio...

CDril by Associate
  • 1095 Views
  • 4 replies
  • 0 kudos