STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SDIO + SD Card + USB MSD .....Windows Problem

Hey everybody,I just got it working that I can use my SD Card as an USB MSD. I can write, read and delete files. Everything looks good.The only problem is that when I connect the USB cable to my computer it takes like 2-3 minutes until the SD card is...

JCorn.2 by Associate II
  • 645 Views
  • 1 replies
  • 0 kudos

IrDA not working on L0-series

Using CubeMX v5.3.0 to generate IrDA on USART2 at both 115200 and 9600 baud doesn't seem to work. I have enabled both the interrupt and DMA in CubeMX and left both pins pulled high. The generated code was then opened in Keil uVision V5.28.0.0 where I...

Erfdd by Associate
  • 754 Views
  • 0 replies
  • 1 kudos

Ethernet Buffer issue.

I need some help. I'm using the STM32F46 with the PHI(LAN8742A) to communicate with Android's Tablet using LWIP. The communication works great, but after sent some data from the tablet to the MCU, the communication collapse. If I increase the size of...

SArma by Associate
  • 1198 Views
  • 0 replies
  • 0 kudos

ethernet with dp83848 on RMII mode

I changed ethernet transceiver chip .My ethernetif.c file works with lan8742 but I have to use dp83848 on my project.I've compare datasheets of two chips and I've edited lan8742.c-h files according to dp83848's datasheet.However it's not work...

Bilge by Associate III
  • 1423 Views
  • 0 replies
  • 0 kudos