Hi -I have a STM32429I-EVAL board. Before I start mucking about with it, I would like the original firmware file (bin or hex file). I may want to go back to the original demo fw at some point. Here is the system info:Demo Rev: 1.4.5Board: STM324x...
The data sheet says the bits allow pressure range and accuracy to be configured, but I'm not seeing how these work. The STM32 Cube example code does not offer any clues. Also in the code, either the comment or setting is not consistent. When the...
I need to get a copy of the STM32CubeF4_1.16.0 firmware and can't find the archived versions on your website. Can you please point me in the right direction?
Posted on March 02, 2018 at 01:35I'm using 2 different ST-LinkV2s to put firmware on a ST32F429ZIT6 processor. I'm using the SWD interface. One of the ST-Links works and the other does not. The one that does not will not even connect to the devic...
Hi -The STM32CubeProgrammer can't save 2 MB. It can only save 1 MB files. The ST-Link Utility can save 2MB files but can only open 1 MB files. I could save the flash contents in 1 MB chunks. But what I'm really interested in is the original FW th...
Posted on March 02, 2018 at 21:29Clive One -Thanks for your response. The fake ST-Link came from one of our vendors and they instucted me to specifically NOT connect pin 1 (which worked for them). I'm glad I took them apart and even happier that y...