STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with programming one STM32F070RB thru another STM32F070RB (connected uarts) using Raspberry pi and stm32flash

Hello everyone,at the start I would like to apologize for my English. It's not the best so I hope that you won't have any dificulties with reading and understanding my problem.I have very strange problem with programming STM32F070RBT.So I am trying t...

DKubi by Associate II
  • 1853 Views
  • 2 replies
  • 0 kudos

Resolved! TIM5 CH4 PWM Output

Hi all,i initialized the TIM5 CH4 PWM with the cube mx interface and then i used :HAL_TIM_PWM_Start(&htim5, TIM_CHANNEL_4);The output is supposed to be observed on PI0 - D5 on the CN4 on the back. There is nothing on the oscilloscope though. Do you k...

AGaru by Associate III
  • 1644 Views
  • 2 replies
  • 0 kudos

USB CDC+MSC Composite Device VID/PID

Posted on February 02, 2015 at 13:03I'm trying to create a USB CDC+MSC composite device using STM32F4 so that it gets automatically recognized by both STM32 CDC driver and as a standard MSC device. Does ST provide a VID/PID pair for such a device? I...

Resolved! How to check vbus is on or off in stm32g4 usb pd?

From the document, the sink will check:A SINK must present an Rd resistor and detection is done in two steps:1. detect the presence of Rp resistor2. detect a VBUS ON.I tested in stm32g431rb, connect ucpd_cc to a power adapter(source), Source send the...

Gbang by Associate III
  • 1668 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.