STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L152 USART3

I tried to use USART3. After few RX/TX messages the port is locked. It stay always into interrupt routine. Only the RX/TX interrupts are handled (activated). Ther is somebody with the similar situation? Thanks.

costi by Associate III
  • 1997 Views
  • 5 replies
  • 0 kudos

Can we save the text file in STM32F373C8 flash and it should detected when connected to computer via USB. Please let me know

Dear all,I want to save my data in the form of text file in the flash memory of the controller STM32F373C8. And it can be retrieve when it is connected to the PC via USB, Is this controller is suitable for my application. If yes please give me the r...

TH U by Associate
  • 840 Views
  • 1 replies
  • 0 kudos

Multiple Sockets with FreeRTOS and LwIP

Hi,I have some code that I have working with FreeRTOS CMSIS v2 and LwIP that creates 2 separate threads, one listens on a TCP port the other listens on a different UDP port. This implementation works fine, however if I change to using CMSIS v1 then t...

DBurr by Senior
  • 1050 Views
  • 0 replies
  • 0 kudos

Ethernet on NUCLEO-F746ZG not working

I'm using a NUCLEO-F746ZG development board and trying to get Ethernet working but so far it isn't even pingable. I'm using STM32CubeIDE and all recommended settings. I've already been able to get Ethernet working on a STM32F746-DISCOVERY. Any sugges...

DBurr by Senior
  • 1756 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.