STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Hi, I'm using stm32L073Rz , need to know how to configure it as a usb memory device, no demo examples are available for usb memory stick for this chip , i used cubemx to generate code for usb memory class and ran it.

It does not work , it gets detected as unknown device,what am i missing , should i add something more to cube mx generated code. Thanks.

svii by Associate III
  • 1517 Views
  • 3 replies
  • 0 kudos

stm32l476 disc uart DMA not working

#include "main.h"#include "uartDma.h"UART_HandleTypeDef huart2;DMA_HandleTypeDef hdma_usart2_tx;void uartStart(void){ MX_DMA_Init(); MX_USART2_UART_Init(); uint8_t pData[] = "This is Polling\r\n"; uint8_t pdata[] = "This is Dma\r\n"; HAL_UART_Tran...

Jagath by Associate II
  • 711 Views
  • 0 replies
  • 0 kudos

STM32F401 USB remote wakeup does not work

Environment:STM32F401RCUSB HID device, Full speedfreeRTOSProblem:Device can send/receive data to/from host and can be put in suspend state and resume from suspend state.However, the remote wake-up function never worksCode:My USB remote wake up log in...

Resolved! STM32L475RG - Having trouble jumping between multiple .bin programs in flash, program stops working.

CURRENT PRODUCT Our existing devices have a custom USB DFU bootloader starting at address 0x08000000. Our main application starts at 0x08008000, after 32Kb of space. I can jump from the main app to the bootloader with no issues (using a NVIC_Systemre...

RSikk.493 by Associate II
  • 1873 Views
  • 5 replies
  • 0 kudos